Configure a fault routine

To execute fault-handling logic when a program fault occurs, configure a routine to be fault routine for the program. Use the
Configuration
tab of the
Program Properties
dialog box to assign a fault routine.
To configure a fault routine:
  1. From either the Controller Organizer or Logical Organizer, right-click the program to change and choose
    Properties
    .
  2. Choose the routine to designate as the fault routine from the
    Fault
    menu in the
    Assigned Routines
    frame.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal