Keyboard operations in Parameters and Connections grid

Use these keys to navigate within the Parameters and Connections grids.
Key
Edit Mode Behavior (focus inside the cell)
Grid Mode Behavior (focus on the grid cell)
Enter
Accepts edit and moves focus down one cell
Moves focus down one cell
Shift + Enter
Accepts edit and moves focus up one cell
Moves focus up one cell
Ctrl + Enter
Accepts edits and leaves focus in current cell
Nothing
Esc
Cancels edits and leaves focus in current cell
Nothing
F2 (text columns only)
Accepts edits and leaves focus in current cell (same as Ctrl + Enter)
Moves focus into cell and selects all text (if appropriate)
Tab
Control specific behavior
Moves focus right one cell
Shift + Tab
Control specific behavior
Moves focus left one cell
Alt + down arrow
Expands cell contents (for example, expands a combo box)
Moves focus into cell and expands cell contents if possible
Shift + F10
Opens the context menu for the cell
Nothing
Arrow keys
Control specific behavior
Moves cell focus in direction of the arrow
Typing text
Control specific behavior
Moves focus into cell, selecting all text, if appropriate, and replacing selected text with the text being keyed in
Ctrl + x
Control specific behavior (selected text is cut)
Nothing
Ctrl + c
Control specific behavior (selected text is copied)
Nothing
Ctrl + v
Control specific behavior (text in clipboard is pasted at cursor location)
Nothing
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal