Save pending edits to execute online command?

Certain commands (Motor/Encoder Test) require saving any pending edits on the current axis before they can execute. Answering Yes lets you continue with the command sequence; answering No aborts the command sequence.
The Motor Test command requires you to observe the direction of axis motion when executed to determine whether the desired positive motion of axis matched the direction of motion when Motor Test was executed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal