New Equipment Phase Dialog Box Overview

Create a new equipment phase program from this dialog box.
The table provides descriptions of the parameters available on this dialog box.
Parameter
Description
Name
Enter a name for the new equipment phase program.
Description
Enter a description of the equipment phase program.
Parent
To make this equipment phase a child of an existing program in the logical model, select the parent program. Otherwise select <none>.
Schedule In
Choose the task for the equipment phase program to be scheduled.
Inhibit Equipment Phase
Select this check box to prevent the equipment phase program and its routines from executing.
Synchronize Redundancy Data after Execution
Choose to synchronize redundancy data after execution (check box is selected) or not to synchronize redundancy data after execution (check box is cleared). The check box is cleared by default.
Note that the check box is not shown for non-Redundancy catalog numbers. The check box is always enabled for controllers with Redundancy enabled. The check box is disabled when Redundancy is not enabled.
OK
Select this button to accept the information entered and create the new equipment phase program.
If online, the equipment phase program is created in the controller.
Cancel
Select this button to cancel the creation of this equipment phase program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal