Search
Studio 5000 Logix Designer Online Help
File menu
The
File
menu contains these commands:
New command
Open command
Close command
Save command
Save As command
New Component > Add-On Instruction command
New Component > Data Type command
New Component > Equipment Phase command
New Component > Equipment Phase State Routine command
New Component > Equipment Sequence command
New Component > Module command
New Component > Program command
New Component > Routine command
New Component > String Type command
New Component > Tag command
New Component > Task command
New Component > Trend command
Import Component > Add-On Instructions
Import Component > Data Type
Import Component > Equipment Phase
Import Component > Program
Import Component > Routine
Import Component > String Type
Import Component > Trend
Compact command
Page Setup command
Generate Report command
Print > Routine command
Print > Routine Properties command
Print > Tags command
Print > Sequencing and Step Tags command
Print > Module Properties command
Print > Add-On Instructions Signatures command
Print > Add-On Instruction command
Print > Data Type command
Print > Cross Reference command
Print > Controller Organizer command
Print > Controller Properties command
Print > Task Properties command
Print > Program Properties command
Print > Equipment Sequence command
Print > Entire Project command
Print Options command
Recent Projects command
Exit command
Studio 5000 Logix Designer
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal