Change the serial configuration online

When you are online and communicating to a controller via a serial connection, any change you make to the connection's attributes will cause the connection to be dropped as soon as the change is applied in the controller.
This message prompts you to confirm whether you wish to continue with the change.
  • If you click Yes, the serial configuration change (if valid) is applied in the controller and the connection will eventually time out.
  • If you click No, nothing happens, and the connection remains in the same state it was in before you attempted to apply the change.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal