Motion Coordinated Transform with Orientation (MCTO)
This information applies to the
Compact GuardLogix
5380, CompactLogix
5380, CompactLogix
5480, ControlLogix
5580, and GuardLogix
5580 controllers.Use the Motion Coordinated Transform with Orientation (MCTO) instruction to establish a bidirectional transform that is set up between a Cartesian and a robot system with coordinates that are joint axes of a robot. The XYZ translation coordinates and the RxRyRz orientation coordinates in the fixed angle convention define the Cartesian coordinates. The geometrical configurations of the robots typically have joint axes that are not orthogonal. The coordinate system type, such as Delta, specifies the geometrical configurations.
Architecture | Standard | Safety |
---|---|---|
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | No | No |
Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers | Yes | No |
This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
MCTO(CartesianSystem, RobotSystem, MotionControl, WorkFrame, ToolFrame);
Operands
IMPORTANT:
Do not use the same tag name for more than one instruction in the same program. Do not write to any instruction output tag under any circumstances.
ATTENTION:
If instruction operands are changed while in Run mode, the pending edits must be accepted and the controller mode cycled from Program to Run for the changes to take effect.
Configuration
The following table provides the operands used to configure the instruction. These operands cannot be changed at runtime.
Operand | Data Type | Format | Description |
---|---|---|---|
Cartesian System | COORDINATE_SYSTEM | tag | Cartesian coordinate system used to program the moves. Reference to Cartesian coordinate system used to program the moves. For controllers that support the REF_TO motion data types, the coordinate system operand type can be replaced by the REF_TO_COORDINATE_SYSTEM type. |
Robot System | COORDINATE_SYSTEM | tag | Non-Cartesian coordinate system that controls the actual equipment. Reference to Non-Cartesian coordinate system that controls the actual equipment. For controllers that support the REF_TO motion data types, the coordinate system operand type can be replaced by the REF_TO_COORDINATE_SYSTEM type. |
Motion Control | MOTION_INSTRUCTION | tag | Control tag for the instruction. |
Work Frame | POSITION_DATA | immediate tag | Work Frame offsets are the offsets used to locate the user Work frame of the Robot relative to the origin of the Robot base frame. These offsets consist of an XYZ and RxRyRz value. This allows the programs to be written in the user work space or world frame and transformed to the Robot base frame. To rotate the target position around the X, Y, or Z axis or offset the target position along the X, Y, or Z axis of the Robot base coordinate system, enter the degrees of rotation into the Rx, Ry, and Rz tag members in units of degrees of rotation, and enter the offset distances into the X, Y, and Z tag members in coordination units. Set the ID member to a value greater than or equal to zero. To maintain the work frame at the robot base frame, leave structure values at zero, or set the operand tag value to zero. |
Tool Frame | POSITION_DATA | immediate tag | Tool Center Point (TCP) offsets are the offsets used to locate the tool center relative to the center of the End of Arm. These offsets consist of an XYZ and RxRyRz value. To have the target position account for an attached tool having translation and/or orientation offsets, enter the tool offset distances into the X, Y, and Z tag members in coordination units. Enter the degrees of tool rotation into the Rx, Ry, and Rz tag members in units of degrees of rotation. Set the ID member to a value greater than or equal to zero. To have the target position reflect only the point at the end-of-arm, leave the structure values at zero, or set the operand tag value to zero. |
For further information of configuring coordinate systems refer to the Motion Coordinate System User Manual publication MOTION-UM002.
IMPORTANT:
Do not write to any instruction output tag under any circumstances.
Affects Math Status Flags
No
Major/Minor Faults
This instruction generates a major fault if an invalid reference or the wrong reference type is provided. A major fault can occur if an uninitialized reference or a reference of incorrect type is passed to Coordinate System operands. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | Same as Rung-condition-in is false. |
Rung-condition-in is false | The .EN, .DN, and .ER are cleared to false. |
Rung-condition-in is true and .EN bit is false | The .EN bit is set to true and the instruction executes. |
Rung-condition-in is true and .EN bit is true | N/A |
Postscan | Same as Rung-condition-in is false. |
Structured Text
Condition/State | Action Taken |
---|---|
Prescan | See Prescan in the Ladder Diagram table. |
Normal execution | See Rung-condition-in is false followed by Rung-condition-in is true in the Ladder Diagram table. |
Postscan | See Postscan in the Ladder Diagram table. |
Data Flow of MCTO instruction between two coordinate systems
Establish the reference frame for the joint coordinate system to ensure the transformations work properly. Refer to the applicable geometry configuration topic for further information on establishing the reference frame for a robot coordinate system.
Once the robot reference frame is established, the robot can be moved to any desired position in joint space when transform is not enabled. When MCTO is initiated for the first time, a forward transform is executed first to set the corresponding Cartesian coordinate positions. Once the MCTO instruction is active, a bidirectional transform link is established, so that if the Cartesian coordinate is commanded to move to a target position in the Cartesian space along a linear path, the robot moves to the Cartesian target coordinates along a linear path. Similarly, if the Robot is commanded to move to a joint coordinate position, the Robot moves to the joint target position along a non-Cartesian path. While MCTO instruction is active, the system maintains the coordinate system related data for Cartesian and Robot coordinate systems.
This diagram illustrates the transformation from a Cartesian coordinate system(X,Y,Z,Rx,Ry,Rz) to a Delta robot geometry with 5 axes (J1J2J3J4J5). The Rx, Ry, and Rz represent orientations around X,Y,Z axes in a positive direction.

Configure an MCTO instruction
The following illustration shows how to configure an MCTO instruction, with the Cartesian coordinate system as the source and the Delta 5 axis geometry as the target. Configure the source and target coordinate systems in the coordinate system dialog box.

Data flow during forward transform when MCTO is active
A forward transform executes when a move executes on joint coordinates of a robot system with an enabled MCTO instruction. During forward transform, the current joint angle positions compute the corresponding Cartesian coordinate positions based on geometry.

Data flow during inverse transform when MCTO is active
When MCTO is active, during inverse transform, the instruction uses the current cartesian positions and geometry configuration to compute the corresponding joint angle positions. MCTO returns an Error 61 when moving both Cartesian and Joint coordinate systems simultaneously.

Fault codes
For the Motion Coordinated Transform with Orientation (MCTO) instruction, an error will occur at runtime if invalid operand values are provided.
Extended Error codes
Extended Error codes help to further define the error message given by the instruction. Their meaning is dependent upon the Error Code with which they are associated.
Error Code | EX_ERROR Code | Description |
---|---|---|
13 | 3 | Value Out Of Range (base angle) Any orientation angle ![]() ![]() |
13 | 3 | Value Out Of Range (base ID) ID equals any negative value. |
13 | 4 | Value Out Of Range (tool angle) Any orientation angle ![]() ![]() |
13 | 4 | Value Out Of Range (tool ID) ID equals any negative value. |
61 | 1 | Connection Conflict: Transform Motion Group Error. Cartesian or Robot coordinate system is ungrouped, or associated to a different motion group from the other. |
61 | 2 | Connection Conflict: Transform Duplicate Systems Error. Operand 0 and Operand 1 are of the same coordinate system type. |
61 | 3 | Connection Conflict: Transform Source Dimension Error. Transform dimension of the Cartesian coordinate system is ![]() |
61 | 4 | Connection Conflict: Transform Target Dimension Error. Robot coordinate system Transform Dimension is equal to zero. |
61 | 5 | Attempting to use the CS as multiple sources - FAN-OUT error. |
61 | 6 | Attempting to use the CS as multiple targets - FAN-IN error. |
61 | 9 | Connection Conflict Transform Axes Overlap Error An axis is a member of both the Cartesian and Robot systems. |
61 | 10 | Axis or axes are in motion with the below exception: Gearing or camming motion is in progress on the Cartesian CS axes. The Cartesian CS slave axes cannot have a master axis from the Robot CS. |
61 | 12 | Connection Conflict Transform Invalid Link Length Link length values for any robot geometry must be ![]() |
61 | 13 | Axis is shut down |
61 | 14 | Axis is inhibited |
61 | 15 | Connection Conflict Transform Invalid Delta Configuration Link Length1 must not be equal to LinkLength2 End Effector Offset1 Re must not be negative For Delta J1J2J6 and Delta J1J2J3J6 End Effector Offset3(D3) must not be negative (Link length 1 + Rb - Re) must be less than link length 2 (Link length 1 + Rb – Re) must be positive or greater than zero |
61 | 18 | Connection Conflict Transform Invalid Articulated Configuration When the offset value is invalid for Articulated Independent J1J2J3J4J5J6 geometry, this error is generated. Base offset Yb must be equal to 0.0 End-Effector offset Ye must be equal to 0.0 End-Effector offset Ze must be equal to 0.0 |
67 | 1 | Invalid Transform Position Invalid Rx Orientation Invalid Rx orientation value at EOA transformations. For 4 axis geometries only Rx = 180 deg position is allowed. For all other positions, it generates an error. |
67 | 2 | Invalid Transform Position Invalid Ry Orientation Invalid Ry orientation value at EOA transformations. For 4 axis geometries, after removing work frame and tool frame, there should not be any Ry orientation values at EOA |
67 | 3 | Invalid Transform Position Invalid Rz Orientation |
147 | 3-5 | Invalid Orientation Scaling Constant Extended error code 3 : Rx Extended error code 4 : Ry Extended error code 5 : Rz Orientation axis has scaling constant ![]() has scaling constant which is not Integer or has Conversion ratio between Coordination Units and Position Units other than 1:1. |
148 | 3-5 | MCPM Orientation Offset Not Rx orientation offset not valid. Extended error code 3 : Rx orientation offset not valid. Extended error code 4 : Ry orientation offset not valid. Extended error code 5 : Rz orientation offset not valid. If robot Geometry is (MO_CD_J1J2J6 or MO_CD_J1J2J3J6) and:
Or if robot Geometry is MO_CD_J1J2J3J4J5 and:
|
149 | 3-5 | Orientation Axis Not Virtual Extended error code 3 : Rx axis must be virtual if transforms are enabled. Extended error code 4 : Ry axis must be virtual if transforms are enabled. Extended error code 5 : Rz axis must be virtual if transforms are enabled. |
151 | 1 | Joint Angle J1 Beyond Limits For details, refer to Geometry related Maximum Joint Limit Section. |
151 | 2 | Joint Angle J2 Beyond Limits For details, refer to Geometry related Maximum Joint Limit Section. |
151 | 3 | Joint Angle J3 Beyond Limits For details, refer to Geometry related Maximum Joint Limit Section. |
151 | 4 | Joint Angle Beyond Limits This indicates the error condition when the Joint 4 in a 5 axis Delta goes beyond turns counter range limit (45899.99 ![]() ![]() Ext Error 4 : Joint J4 Beyond Limit |
151 | 5 | Joint Angle Beyond Limits This indicates error condition when the Joint 5 in a 5 axis Delta goes beyond +/-179, +179 ![]() ![]() Ext Error 5 : Joint J5 Beyond Limit |
151 | 6 | Joint Angle Beyond Limits This indicates the error condition when the Joint 6 in a 4 axis Delta goes beyond turns counter range limit (45899.99<J6<-45900) Ext Error 6 : Joint J6 Beyond Limit |
152 | 1 | Maximum Orientation Speed Exceed for Rx When Orientation axis Rx is commanded to move by an angle greater than or equal to 180 degrees in one coarse update period, this error and extended error is returned. |
152 | 2 | Maximum Orientation Speed Exceed for Ry When Orientation axis Ry is commanded to move by an angle greater than or equal to 180 degrees in one coarse update period, this error and extended error is returned. |
152 | 3 | Maximum Orientation Speed Exceed for Rz When Orientation axis Rz is commanded to move by an angle greater than or equal to 180 degrees in one coarse update period, this error and extended error is returned. |
153 | 1 | Invalid Translation Position MOP Invalid X Translation Translation on X axis is Invalid |
153 | 2 | Invalid Translation Position MOP Invalid Y Translation Translation on Y axis is Invalid |
153 | 3 | Invalid Translation Position MOP Invalid Z Translation Translation on Z axis is Invalid |
156 | 1 | Singularity Condition Error Joint 1 axis is close to Arm Singularity condition in Articulated Independent J1J2J3J4J5J6 Geometry Ext Error 1: Arm Singularity Condition |
156 | 2 | Singularity Condition Error Joint 3 axis is close to Elbow Singularity condition in Articulated Independent J1J2J3J4J5J6 Geometry Ext Error 2: Elbow Singularity Condition |
156 | 3 | Singularity Condition Error Joint 5 axis is close to Wrist Singularity condition in Articulated Independent J1J2J3J4J5J6 Geometry Ext Error 1: Wrist Singularity Condition |
Example
The following examples activate the transformations between Cartesian coordinate system CS1 and robot coordinate system CS2, which is a Delta 5 axis geometry. In the first example, neither work frame nor tool frame are specified, so Cartesian positions are computed at robot end-of-arm (EOA), with respect to the robot base frame.
Ladder Diagram

When MCTO is active, with a move to Cartesian positions X = 7.361, Y = -4.25, Z = -928.18, Rx = 180, Ry = 30 and Rz = -30, the MCTO computes the corresponding Joint angle as shown in the following diagram.

Consider the same MCTO, with work frame offsets enabled for X = 50, Y = 50 and Rz = 50. Now MCTO will compute the Cartesian positions with respect to the new work frame.

When a move is programmed to the same end position, the corresponding joint positions are as shown in this diagram.

Consider that the MCTO is programmed with tool frame offsets also enabled for Ry = 50 along with the work frame offsets. MCTO now computes the Cartesian positions with respect to the end of the new work frame and tool frame.

This diagram shows the corresponding Joint angle positions after programming a move to the same end position.

For more information on configuring offsets, see Configure Coordinate System Offsets.
Structured Text
MCTO(CS1, CS2, MCTO1, 0, 0);
TIP:
For further information on creating geometries with orientation support, see the Motion Coordinate System User Manual publication MOTION-UM002.
Provide Feedback