Configure the axis properties

After adding the drive and creating the axes, use the
Axis Properties
dialog box to configure and edit the axis properties for the drive. This dialog box is intended for an expert user who is accustomed to editing an axis.
To configure the axis properties:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, and double-click the axis.
  2. Select the various pages of the
    Axis Properties
    dialog box to make the appropriate changes.
    TIP:
    Whenever there are pending edits on a tab, an asterisk (*) appears next to the page title to indicate pending edits.
  3. Select the
    Apply
    button to save all the pending edits.
    If there are any errors detected, a message box appears indicating the error(s) and returns the focus to the field or item in question.
  4. Select
    OK
    to close the
    Axis Properties
    dialog box, or select
    Cancel
    to reject all pending edits and close the
    Axis Properties
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal