Torque/Current Loop page

Use the settings on the
Torque/Current Loop
page in the Axis Properties dialog box to configure the torque and current loop of the axis.
TIP: To open the Torque/Current Loop page:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, then right-click the axis and select
    Properties
    .
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , select
    Torque/Current Loop
    .
Parameter
Description
Gains Bandwidth
Enter a value for the bandwidth in Hertz.
Integral Time Constant
Enter a value for the integral time constant in seconds.
Peak Torque Limit Positive
Enter a value for the positive peak current limit as a percent rated of the motor.
Peak Torque Limit Negative
Enter a value for the negative peak current limit as a percent rated of the motor.
Motor Overload Limit
Enter a value for the motor overload limit as a percent rated of the motor.
Parameters
Opens the
Motion Axis Parameters
page to modify existing or additional parameters.
Tip:
The
Parameter List
page may contain more attributes than the associated page. In some cases, attributes that display on the
Parameter List
page do not display on the associated page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal