Friction page

Use the settings on the
Friction
page to:
  • Enter the percentage of sliding friction for the load of the motor.
  • Enter the friction compensation window position.
TIP: To open the Friction page:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, and double-click an axis.
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , expand the
    Load
    folder, and then click
    Friction
    .
These are the
Friction
page parameters.
Parameter
Description
Sliding Friction Compensation
Specifies the percentage of sliding friction for the load in % Rated units.
Compensation Window
Specifies the compensation window position in terms of user define position units.
Parameters
Opens the
Motion Axis Parameters
page to modify existing or additional parameters.
Tip:
The
Parameter List
page may contain more attributes than the associated page. In some cases, attributes that display on the
Parameter List
page do not display on the associated page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal