Conversion Constant and Drive Resolution Attributes

The settings for certain axis attributes come from the settings of the Conversion Constant (set on the Conversion tab), or the Drive Resolution (set on the Drive tab).
When you edit the setting for either the Conversion Constant or the Drive Resolution, and then click either
OK
or
Apply
, you must choose whether to also recalculate the settings for these dependent attributes.
If you choose
Yes
, the controller recalculates the settings for the following attributes:
On this tab or dialog:
These attributes are recalculated:
Dynamics tab
Maximum Velocity
Maximum Acceleration
Maximum Deceleration
Limits tab
Position Error Tolerance
Custom Drive Scaling Attributes dialog
Torque Scaling
Custom Limit Attributes dialog
Velocity Limit Bipolar
Velocity Limit Positive
Velocity Limit Negative
Acceleration Limit Bipolar
Acceleration Limit Positive
Acceleration Limit Negative
If you choose
No
, the settings for these attributes remain unchanged.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal