Requirements for Timely Response to Events
Product | Required to Meet IEC-62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® AssetCentre software | Yes | Configure and use the following:
For more information, see the following:
|
Syslog collector | Yes, if not using FactoryTalk AssetCentre for logging | The Drive supports syslog event logging. Choose a syslog collector that supports the following:
IMPORTANT: The drive sends events to a syslog collector through its Ethernet port. The Ethernet port must be connected to the same network as the syslog collector. To set the IP address of the syslog collector, use FactoryTalk® Policy Manager software. For more information, see CIP Security with Rockwell Automation Products Application Technique, publication SECURE-AT001.To view a list of syslog messages and their descriptions, see PowerFlex Drives with TotalFORCE Control Conditions Reference Data, publication 750-RD102. |
Provide Feedback