Requirements for System Integrity
Product | Required to Meet IEC-62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® AssetCentre softwareFactoryTalk® Services Platform (includes FactoryTalk® Security , FactoryTalk® Diagnostics) | Yes | The FactoryTalk® AssetCentre server centrally tracks and manages configuration changes and restricts who can make changes based on FactoryTalk® Security settings. This server functionality assists with diagnostics and troubleshooting and reduces maintenance time for production assets.Configure the feature security for users to limit access to action such as triggering download of DeviceLogix™ (applicable for I/O mode only) program, downloading firmware to the drive and configure the Device Monitor - Change Detect operation. For more information, see Configure System Security Features User Manual, publication SECURE-UM001.Configure the routing and logging option of the FactoryTalk® Diagnostics. Monitor security-related events by setting up audit policies. For more information, see FactoryTalk Security System Configuration Guide, publication FTSEC-QS001. |
FactoryTalk® Policy Manager | Yes | FactoryTalk® Policy Manager is a secure configuration tool that is one of a set of products that Rockwell Automation® uses to implement CIP Security™ .CIP Security™ helps to provide a secure data transport across an EtherNet/IP™ network. Use FactoryTalk® Policy Manager software to create zones and turn on CIP Security™ to differentiate trusted and untrusted devices.For more information, see CIP Security with Rockwell Automation Products, publication SECURE-AT001. |
Secure DPI Ports | Yes | Applicable for I/O mode only: HIM and Communication option cards are connected to the drive through DPI ports and should be secured by configuring the mask parameters in the drive. After product commissioning, HIM should be either removed or set to read-only mode. To remove HIM, see instruction on PowerFlex 20-HIM-A6 and 20-HIM-C6S HIM User Manual, publication 20HIM-UM001. Communication option cards should also be disallowed from controlling the logic command (start, jog, change of direction, and so forth) of the drive. The following mask parameters can be used to configure the control to logic command and to set read-only mode:
For more information, see CIP Security with Rockwell Automation Products, publication SECURE-AT001. Applicable for CIP™ Motion mode only:HIM can only be used for monitoring and cannot be used to control the drive or change configuration settings. For more information, see Integrated Motion on the EtherNet/IP Network: Configuration and Startup User Manual, publication MOTION-UM003. |
Limit physical access to drive and its HIM | Yes | Actively managed physical access to the drive and its HIM. Secure physical access to the drive and HIM by limiting physical access through locked cabinets and raising awareness of threats through training and communication to personnel. For more information, see System Security Design Guidelines Reference Manual, publication SECURE-RM001. |
ControlFLASH Plus® or ControlFLASH™ software | Yes | Use ControlFLASH Plus® or ControlFLASH™ software to update drive firmware. Digitally signed firmware files have a DMK (Device Management Kit) extension. ControlFLASH™ software authenticates the origin of a DMK file and validates the file before download in the device. |
Digitally signed firmware | Yes | To meet IEC-62443-4-2 SL 1 security requirements, you must use a certified version of the TotalFORCE® Control drive firmware revision 13.002 or later. We recommend that you use the latest revision from Rockwell Automation official download portal Product Compatibility & Download Center at . |
User-configurable fault handling | Yes | Applicable for I/O mode only: There are 5 fault action options (fault, stop, zero data, hold last and send Flt Cfg) available that can be set when certain fault occurs. Configure based on use case if the default action (fault) is not suitable. Configure based on use case if the default action (fault) is not suitable. For more information, see PowerFlex Drives with TotalFORCE Control Built-in EtherNet/IP Adapter User Manual, publication 750COM-UM009. Applicable for CIP™ Motion mode only:Configure actions for faults through Studio 5000 Logix Designer® . For more information, see Integrated Motion on EtherNet/IP Networks for PowerFlex 755T Products with TotalFORCE Control Application Technique, publication 750-AT007. |
Provide Feedback