Requirements for Resource Availability
Product | Required to Meet IEC-62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® AssetCentre software | Yes | Configure and use the following:
For more information, see the following:
|
CIP Security™ | Yes | Configure FactoryTalk® Policy Manager software to define the zones, devices, and conduits for secure data transport through CIP Security™ .CIP Security™ shall be enabled for the devices within a security zone and each device identity shall be authenticated with a pre-shared key or certificate.For more information, see the following:
|
Automatic Device Configuration (ADC) | Yes | Applicable for I/O mode only: Enable the ADC feature to allow the controller to automatically load the saved drive parameter settings into a drive on Ethernet/IP connection establishment if the controller detects a difference with the saved configuration. For more information, refer to the PowerFlex Drives with TotalFORCE Control Built-in EtherNet/IP Adapter, publication 750COM-UM009. |
CopyCat | Yes, if ADC is not enabled | Applicable for I/O mode only: The drives support CopyCat function that allows user to upload individual or multiple parameters set for the host drive or any of its connected peripherals into the HIM. For more information, see the PowerFlex 20-HIM-A6 and 20-HIM-C6S HIM (Human Interface Module) User Manual, publication 20HIM-UM001. |
Studio 5000 Logix Designer® application | Yes, if ADC is not enabled | Drive configuration settings, including drive parameters, can be kept in the controller project file (.ACD). For more information, see PowerFlex Drives with TotalFORCE Control Built-in EtherNet/IP Adapter, publication 750COM-UM009. |
Restrict Unused Open Ports | Yes | To restrict the unused open ports, user is required to identify the open ports and send CIP command with TCP/IP Interface object (0xF5) and services code as below: 0x4C: To configure the state (open / closed) of a specific port number. 0x4D: To configure the state (enabled / disabled) of a specific protocol number. For more information, see PowerFlex Drives with TotalFORCE Control Built-in EtherNet/IP Adapter, publication 750COM-UM009. |
Provide Feedback