Drive Security Features
For
PowerFlex®
755T products to comply with the certification requirements, implement the control system with these other security-focused products.Security-focused Control System
Item | Description |
|---|---|
A | Domain Controller |
B | FactoryTalk® Directory Server |
C | FactoryTalk® AssetCentre Server |
D | FactoryTalk® View SE Server |
E | Syslog Collector |
F | PowerFlex® 755T Drive |
G | ControlLogix® 5580 Controller, 1756-EN4T EtherNet/IP™ Communication Module |
H | Stratix® 5400 Switch |
Studio 5000 Logix Designer® , ControlFLASH Plus™ or ControlFLASH™ software | |
J | FactoryTalk® View SE Client |
Security Checklists
Follow the security checklists in this chapter to secure the system and the drive. It is your responsibility to monitor the system periodically to make sure that the security settings function as you configured them.
Provide Feedback