Safety Instructions
Mnemonic | Name | Description |
|---|---|---|
CROUT | Configurable Redundant Output | Controls and monitors redundant outputs. |
DCA | Dual Channel Input - Analog (integer version) | Monitors two analog values for deviation and range tolerance. |
DCAF | Dual Channel Input - Analog (floating point version) | Monitors two analog values for deviation and range tolerance. |
DCM | Dual Channel Input - Monitor | Monitors dual-input safety devices. |
DCS | Dual Channel Input - Stop | Monitors dual-input safety devices whose main purpose is to provide a stop function, such as an E-stop, light curtain, or gate switch. |
DCSRT | Dual Channel Input - Start | Energizes dual-input safety devices whose main function is to start a machine safely, for example an enable pendant. |
DCST | Dual Channel Input - Stop With Test | Monitors dual-input safety devices whose main purpose is to provide a stop function, such as an E-stop, light curtain, or gate switch. It includes the added capability to initiate a functional test of the stop device. |
DCSTL | Dual Channel Input - Stop With Test and Lock | Monitors dual-input safety devices whose main purpose is to provide a stop function, such as an E-stop, light curtain, or gate switch. It includes the added capability to initiate a functional test of the stop device. It can monitor a feedback signal from a safety device and issue a lock request to a safety device. |
DCSTM | Dual Channel Input - Stop With Test and Mute | Monitors dual-input safety devices whose main purpose is to provide a stop function, such as an E-stop, light curtain, or gate switch. It includes the added capability to initiate a functional test of the stop device and the ability to mute the safety device. |
FSBM | Four Sensor Bi-directional Muting | Automatically disables the protective function of a light curtain temporarily, by using four sensors that are arranged sequentially before and after the sensing field of the light curtain. |
SMAT | Safety Mat | Indicates whether the safety mat is occupied. |
THRSe | Two-Hand Run Station – Enhanced | Monitors two diverse safety inputs, one from a right-hand push button and one from a left-hand push button, to control one output. Features configurable channel-to- channel discrepancy time and enhanced capability for bypassing a two-hand run station. |
TSAM | Two Sensor Asymmetrical Muting | Automatically disables the protective function of a light curtain temporarily, by using two muting sensors that are arranged asymmetrically. |
TSSM | Two Sensor Symmetrical Muting | Automatically disables the protective function of a light curtain temporarily, by using two muting sensors that are arranged symmetrically. |
Provide Feedback