Diagnostic Channels
Diagnostic IO-Link Master Channel
- Size = 48 bytes
The following Data Types must be retrieved as part of the Diagnostic Assembly
Instance.
Follow the information in the following table to add each member.
Name | Data Type | Size in Bytes |
|---|---|---|
Fault | BOOL | 2 |
Uncertain | BOOL | |
NoLoad | BOOL | |
ShortCircuit | BOOL | |
DiagBit_Pad5 | BOOL | |
FieldPowerOff | BOOL | |
DiagBit_Pad7 | BOOL | |
DiagBit_Pad8 | BOOL | |
DiagBit_Pad9 | BOOL | |
SSVShortCircuit | BOOL | |
DiagBit_Pad11 | BOOL | |
DiagBit_Pad12 | BOOL | |
DiagBit_Pad13 | BOOL | |
DiagBit_Pad14 | BOOL | |
DiagBit_Pad15 | BOOL | |
PortStatusInfo | USINT | 1 |
Pad1 | SINT | 1 |
Pad2 | DINT | 4 |
NoLoadTimstamp | SINT | 8 |
ShortCircuitTimestamp | SINT | 8 |
FieldPowerOnTimestamp | SINT | 8 |
FieldPowerOffTimestamp | SINT | 8 |
SSVShortCircuitTimestamp | SINT | 8 |
Provide Feedback