Windows View
Windows show a summary of the module windows configuration.
Windows View Example

The Windows view includes these parameters:
Parameter | Description |
|---|---|
Window | Displays the window number to which this configuration
applies. |
Mode | Displays which input tag value the window operates on. |
Unit | Displays the unit that is associated with the configured Mode for
the window. |
Output On Value | Displays the value that defines one side of the window
thresholds. The outputs (if tied to the window) and
I.Windowxx.InWindow tag switch state at this
threshold according to the diagram Figure 1. |
Output Off Value | |
Output On Hysteresis | Displays the negative offset from the Output On Value to apply
hysteresis to. |
Output Off Hysteresis | Displays the negative offset from the Output Off Value to apply
hysteresis to. |
Provide Feedback