Outputs View
Use Outputs to view or configure the outputs for the device.
Outputs View Example

The Outputs view includes these parameters:
Parameter | Description |
|---|---|
Output | Displays the output number to which this configuration
applies. |
Mode | Displays the mode for the output. |
Output State in Program Mode | Determines the behavior of each output when the controller
transitions to Program Mode or Inhibit mode. While in Program
Mode or Inhibit mode, outputs from the controller are ignored
and the output behaves as follows:
|
Output State in Communication Fault Mode | Determines what happens to the output of each point after a
communication fault occurs and the module enters Communication
Fault Mode.
|
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Outputxx Diagnostics
To view the Outputxx diagnostics, select Diagnostics Outputs view.
Outputxx Diagnostics Example

Provide Feedback