Counter – Fault/Program Actions View
Use Counter– Fault/Program Actions to configure the behavior of the counter when the
module is in Program mode or Fault mode, or when a communication fault occurs.
Counter – Fault/Program Actions View Example

The Counter – Fault/Program Actions view includes these parameters:
Parameter | Description |
|---|---|
Counter State in Program Mode | Determines the behavior of the counter when the controller
transitions to Program Mode or Inhibit mode. While in Program
Mode or Inhibit mode, counters from the controller are ignored
and the counter behaves as follows:
|
Counter State in Program Mode User-defined Value | Defines the value that is set to count when Counter State in
Program Mode is selected as User-defined value. |
Reset stored values in Program Mode | Determines whether to reset the stored values when the controller
transitions to Program Mode or Inhibit mode. |
Counter State in Communication Fault Mode | Determines what happens to the counter after a communication
fault occurs and the module enters Communication Fault Mode.
|
Counter State in Communication Fault Mode User-defined Value | Defines the value that is set to count when Counter State in
Communication Fault Mode is selected as User-defined value. |
Reset stored values in Communication Fault Mode | Determines whether to reset the stored values after a
communication fault occurs and the module enters Communication
Fault Mode. |
When Communication Fails in Program Mode | Determines the counter action if communication fails in Program
Mode.
|
Provide Feedback