Connection View
Use Connection to define controller-to-device behavior:
- Set the RPI rate. For more information, see Requested Packet Interval.
- Select Unicast or Multicast connection to use on the EtherNet/IP network. For more information, see Unicast or Multicast Connection.
- View the reason of Connection Fault.TIP: If there is a connection fault, Connection Fault area displays the error code with description that helps you to troubleshoot the module. For more information, see Troubleshoot Your Module.
- Inhibit the module. For more information, see Module Inhibiting.
- Configure fault response for connection failure while the controller is in Run Mode.
- Enable or disable the Automatic Diagnostics.ATTENTION: If you do not enable Automatic Diagnostics, the device does not publish diagnostics to FactoryTalk Alarms and Events.
Connection View Example

Recommended Minimum RPI Values for Notch Filters
In the following table, each Notch Filter setting has recommended minimum module RPI
value that allow the required time to collect samples from each channel. The
recommended minimum RPI for the module is the maximum one of all recommended values
per channel.
Notch Filter (Hz) | Recommended Minimum Module RPI
Value | |
|---|---|---|
10 | 106 | |
20 | 53.1 | |
50 | 22 | |
60 (default) | 18.3 | |
100 | 9 | |
200 | 5.9 | |
500 | 2.2 | |
1000 | 1.1 | |
2500 | 0.5 | |
5000 | 0.3 | |
Provide Feedback