Documentation Languages toolbar
Use the Documentation Languages toolbar to associate the project's documentation with a language.

Use the Documentation Languages toolbar to switch the currently used documentation language. Change the selection in the
Current Language
box to dynamically change the language used to display all project documentation. This toolbar is the quickest, most convenient way to switch a language dynamically in the project.Use this toolbar to select languages that do not currently have content. If no default language is chosen, the result is blank project documentation for the project.
Languages with content are marked with this icon, indicating that the language has documentation associated with it. | |
![]() | The Documentation Languages button opens the Project Documentation Language Configuration dialog box. |
Unless a current language has been specified,
Select a Language
appears in the Current Language
box. Otherwise, the last language used in the project appears.Provide Feedback