Delete the trend <trend name>?

When you attempt to delete a trend, you are prompted to confirm the deletion. Select
Yes
to remove the trend from the controller; otherwise, select
No
and the deletion is canceled.
If a trend is running when you make a deletion request, the trend is first stopped and then deleted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal