Error Codes
The Logix Designer application does not always display the full description.
Error Code (Hex) | Description | Display In Software |
|---|---|---|
0001 | Connection failure (extended error codes) | Same as description |
0002 | Insufficient resource | |
0003 | Invalid value | |
0004 | IOI syntax error (see extended error codes) | |
0005 | Destination unknown, class unsupported, instance undefined or structure element undefined (see extended error codes) | |
0006 | Insufficient packet space | |
0007 | Connection lost | |
0008 | Service unsupported | |
0009 | Error in data segment or invalid attribute value | |
000A | Attribute list error | |
000B | State already exists | |
000C | Object model conflict | |
000D | Object already exists | |
000E | Attribute cannot be set | |
000F | Permission denied | |
0010 | Device state conflict | |
0011 | Reply will not fit | |
0012 | Fragment primitive | |
0013 | Insufficient command data | |
0014 | Attribute not supported | |
0015 | Too much data | |
001A | Bridge request too large | |
001B | Bridge response too large | |
001C | Attribute list shortage | |
001D | Invalid attribute list | Same as description |
001E | Embedded service error | |
001F | Connection related failure (see extended error codes) | |
0022 | Invalid reply received | |
0025 | Key segment error | |
0026 | Invalid IOI error | |
0027 | Unexpected attribute in list | |
0028 | DeviceNet error - invalid member ID | |
0029 | DeviceNet error - member not settable | |
00D1 | Module not in run state | Unknown error |
00FB | Message port not supported | |
00FC | Message unsupported data type | |
00FD | Message uninitialized | |
00FE | Message timeout | |
00FF | General error (see extended error codes) |
Provide Feedback