Simultaneous Branch Diverge
The simultaneous diverge branch represents two or more alternate paths of execution.
In a simultaneous branch, all alternate paths are executed in parallel.
Available Languages
Ladder Diagram |
Not Available |
Function Block |
Not Available |
Sequential Function Chart |
![]() |
Structured Text |
Not Available |
Description
A simultaneous branch represents steps or group of steps that occur at the same time (that is, an AND structure).
- All branches execute.
- All branch must finish before continuing with the SFC.
- The controller checks the transition after the last step of each branch has executed at least once.

Provide Feedback