Select Branch Diverge
The selection diverge branch represents two or more alternate paths of execution.
In a selection branch, only one alternate path is executed depending on which transition condition is true.
Available Languages
Ladder Diagram |
Not Available |
Function Block |
Not Available |
Sequential Function Chart |
![]() |
Structured Text |
Not Available |
Description
A selected branch represents a choice between one step or group of steps or another step or group of steps (that is, an OR structure).
- Only one branch executes.
- By default the controller checks the transitions from left to right.
- The controller takes the first true branch.
- TheLogix Designerapplication lets you change the order in which the controller checks the transitions.

Provide Feedback