Process Multi Sensor Analog Input (PAIM)
This information applies to the CompactLogix 5380P and ControlLogix 5580P controllers.
The Process Multi Sensor Analog Input (PAIM) instruction monitors one analog process variable (PV) by using up to eight analog input signals from sources such as sensors, transmitters, and input channels. The PAIM instruction has functions for input selection, averaging, and failure detection. Additional functions, such as filtering and alarming, are done by a downstream PAI block.
The PAIM instruction provides:
- Configuration to use between two and eight input signals.
- Input Source and Quality monitoring of inputs, plus monitoring of each signal for out of range condition. Rejection from the PV calculation of inputs that are out of range, flagged as bad, infinite, or not a number (floating-point exception values).
- Calculation of the average (mean) or median of the inputs in use as the PV value.
- Selectable rejection from the PV calculation of inputs that are outside tau standard deviations from the mean, with a minimum of four required inputs, or inputs that are outside a user-defined deviation from the mean.
- Configuration of the minimum number of good, unrejected input signals required to have a good PV value, and an alarm if the required number of good inputs is not met.
- Configuration of which PV to use if there are only two unrejected signals remaining: the lesser, the greater, or the average of the two.
- An alarm if any inputs configured to be used are rejected.
- An alarm if the number of unrejected inputs is equal to the minimum number required to be good, meaning the next input failure results in a PV failure.
- Display elements, plus a faceplate with bar graph PV indication, mode selection, alarm limit entry and alarm display, configuration, acknowledgment, trending, and maintenance and engineering configuration and setup.
Available Languages
Ladder Diagram

Function Block Diagram

Structured Text
PAIM (PAIMTag, 0);
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Configuration Operands
Operand | Type | Format | Description |
|---|---|---|---|
PlantPAx Control | P_ANALOG_INPUT_MULTI | tag | Data structure required for proper operation of instruction. |
BusObj | BUS_OBJ | tag | Bus component |
P_ANALOG_INPUT_MULTI Structure
Public members are standard, visible tag members that are programmatically accessible. Private, hidden members are used in HMI faceplates and are not programmatically accessible. Private members are listed in separate tables after public members.
Public Input Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
|---|---|---|---|---|---|
EnableIn | BOOL | Not Visible | Not Required | Input | Enable Input - System Defined Parameter Default is true. |
Inp_InitializeReq | BOOL | Not Visible | Not Required | Input | 1 = Request to initialize the instruction. The instruction is normally initialized in instruction first run. Use this request when reinitialization is needed. The instruction clears this operand automatically. Default is true. |
Inp_PVAData | REAL | Visible | Not Required | Input | PV signal from sensor or input A (PV units). Valid = any float. Default is 0.0. |
Inp_PVASrcQ | SINT | Not Visible | Not Required | Input | Input source and quality, from channel A object, if available (enumeration). Default is 0. |
Inp_PVANotify | SINT | Not Visible | Not Required | Input | Related PV object alarm priority and acknowledgement status. 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. Default is 0. |
Inp_SmartDvcASts | DINT | Not Visible | Not Required | Input | Current code provided by SMART device on Inp_PVAData. The code is copied to Out_SmartDvcSts allowing a user to monitor the device status on HMI for diagnostic lookup purposes. Valid = 0 to maximum positive number. Default is 0. |
Inp_PVBData | REAL | Visible | Not Required | Input | PV signal from sensor or input B (PV units). Valid = any float. Default is 0.0. |
Inp_PVBSrcQ | SINT | Not Visible | Not Required | Input | Input source and quality, from channel B object, if available (enumeration). Default is 0. |
Inp_PVBNotify | SINT | Not Visible | Not Required | Input | Related PV object alarm priority and acknowledgement status. 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. Default is 0. |
Inp_SmartDvcBSts | DINT | Not Visible | Not Required | Input | Current code provided by SMART device on Inp_PVBData. The code is copied to Out_SmartDvcSts allowing a user to monitor the device status on HMI for diagnostic lookup purposes. Valid = 0 to maximum positive number. Default is 0. |
Inp_PVCData | REAL | Visible | Not Required | Input | PV signal from sensor or input C (PV units). Valid = any float. Default is 0.0. |
Inp_PVCSrcQ | SINT | Not Visible | Not Required | Input | Input source and quality, from channel C object, if available (enumeration). Default is 0. |
Inp_PVCNotify | SINT | Not Visible | Not Required | Input | Related PV object alarm priority and acknowledgement status. 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. Default is 0. |
Inp_SmartDvcCSts | DINT | Not Visible | Not Required | Input | Current code provided by SMART device on Inp_PVCData. The code is copied to Out_SmartDvcSts allowing a user to monitor the device status on HMI for diagnostic lookup purposes. Valid = 0 to maximum positive number. Default is 0. |
Inp_PVDData | REAL | Not Visible | Not Required | Input | PV signal from sensor or input D (PV units). Valid = any float. Default is 0.0. |
Inp_PVDSrcQ | SINT | Not Visible | Not Required | Input | Input source and quality, from channel D object, if available (enumeration). Default is 0. |
Inp_PVDNotify | SINT | Not Visible | Not Required | Input | Related PV object alarm priority and acknowledgement status. 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. Default is 0. |
Inp_SmartDvcDSts | DINT | Not Visible | Not Required | Input | Current code provided by SMART device on Inp_PVDData. The code is copied to Out_SmartDvcSts allowing a user to monitor the device status on HMI for diagnostic lookup purposes. Valid = 0 to maximum positive number. Default is 0. |
Inp_PVEData | REAL | Not Visible | Not Required | Input | PV signal from sensor or input E (PV units). Valid = any float. Default is 0.0. |
Inp_PVESrcQ | SINT | Not Visible | Not Required | Input | Input source and quality, from channel E object, if available (enumeration). Default is 0. |
Inp_PVENotify | SINT | Not Visible | Not Required | Input | Related PV object alarm priority and acknowledgement status. 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. Default is 0. |
Inp_SmartDvcESts | DINT | Not Visible | Not Required | Input | Current code provided by SMART device on Inp_PVEData. The code is copied to Out_SmartDvcSts allowing a user to monitor the device status on HMI for diagnostic lookup purposes. Valid = 0 to maximum positive number. Default is 0. |
Inp_PVFData | REAL | Not Visible | Not Required | Input | PV signal from sensor or input F (PV units). Valid = any float. Default is 0.0. |
Inp_PVFSrcQ | SINT | Not Visible | Not Required | Input | Input source and quality, from channel F object, if available (enumeration). Default is 0. |
Inp_PVFNotify | SINT | Not Visible | Not Required | Input | Related PV object alarm priority and acknowledgement status. 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. Default is 0. |
Inp_SmartDvcFSts | DINT | Not Visible | Not Required | Input | Current code provided by SMART device on Inp_PVFData. The code is copied to Out_SmartDvcSts allowing a user to monitor the device status on HMI for diagnostic lookup purposes. Valid = 0 to maximum positive number. Default is 0. |
Inp_PVGData | REAL | Not Visible | Not Required | Input | PV signal from sensor or input G (PV units). Valid = any float. Default is 0.0. |
Inp_PVGSrcQ | SINT | Not Visible | Not Required | Input | Input source and quality, from channel G object, if available (enumeration). Default is 0. |
Inp_PVGNotify | SINT | Not Visible | Not Required | Input | Related PV object alarm priority and acknowledgement status. 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. Default is 0. |
Inp_SmartDvcGSts | DINT | Not Visible | Not Required | Input | Current code provided by SMART device on Inp_PVGData. The code is copied to Out_SmartDvcSts allowing a user to monitor the device status on HMI for diagnostic lookup purposes. Valid = 0 to maximum positive number. Default is 0. |
Inp_PVHData | REAL | Not Visible | Not Required | Input | PV signal from sensor or input H (PV units). Valid = any float. Default is 0.0. |
Inp_PVHSrcQ | SINT | Not Visible | Not Required | Input | Input source and quality, from channel H object, if available (enumeration). Default is 0. |
Inp_PVHNotify | SINT | Not Visible | Not Required | Input | Related PV object alarm priority and acknowledgement status. 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. Default is 0. |
Inp_SmartDvcHSts | DINT | Not Visible | Not Required | Input | Current code provided by SMART device on Inp_PVHData. The code is copied to Out_SmartDvcSts allowing a user to monitor the device status on HMI for diagnostic lookup purposes. Valid = 0 to maximum positive number. Default is 0. |
Inp_PVABad | BOOL | Not Visible | Not Required | Input | Signal quality or communication status for input A 1 = Bad, 0 = OK. Default is false. |
Inp_PVAUncertain | BOOL | Not Visible | Not Required | Input | Signal quality for input A, 1 = Uncertain, 0 = OK. Default is false. |
Inp_SmartDvcADiagAvailable | BOOL | Not Visible | Not Required | Input | 1 = SMART device on Inp_PVAData diagnostics available. Typically used to indicate device requires action to keep operating as expected. Default is false. |
Inp_PVBBad | BOOL | Not Visible | Not Required | Input | Signal quality or communication status for input B 1 = Bad, 0 = OK. Default is false. |
Inp_PVBUncertain | BOOL | Not Visible | Not Required | Input | Signal quality for input B, 1 = Uncertain, 0 = OK. Default is false. |
Inp_SmartDvcBDiagAvailable | BOOL | Not Visible | Not Required | Input | 1 = SMART device on Inp_PVBData diagnostics available. Typically used to indicate device requires action to keep operating as expected. Default is false. |
Inp_PVCBad | BOOL | Not Visible | Not Required | Input | Signal quality or communication status for input C 1 = Bad, 0 = OK. Default is false. |
Inp_PVCUncertain | BOOL | Not Visible | Not Required | Input | Signal quality for input C, 1 = Uncertain, 0 = OK. Default is false. |
Inp_SmartDvcCDiagAvailable | BOOL | Not Visible | Not Required | Input | 1 = SMART device on Inp_PVCData diagnostics available. Typically used to indicate device requires action to keep operating as expected. Default is false. |
Inp_PVDBad | BOOL | Not Visible | Not Required | Input | Signal quality or communication status for input D 1 = Bad, 0 = OK. Default is false. |
Inp_PVDUncertain | BOOL | Not Visible | Not Required | Input | Signal quality for input D, 1 = Uncertain, 0 = OK. Default is false. |
Inp_SmartDvcDDiagAvailable | BOOL | Not Visible | Not Required | Input | 1 = SMART device on Inp_PVDData diagnostics available. Typically used to indicate device requires action to keep operating as expected. Default is false. |
Inp_PVEBad | BOOL | Not Visible | Not Required | Input | Signal quality or communication status for input E 1 = Bad, 0 = OK. Default is false. |
Inp_PVEUncertain | BOOL | Not Visible | Not Required | Input | Signal quality for input E, 1 = Uncertain, 0 = OK. Default is false. |
Inp_SmartDvcEDiagAvailable | BOOL | Not Visible | Not Required | Input | 1 = SMART device on Inp_PVEData diagnostics available. Typically used to indicate device requires action to keep operating as expected. Default is false. |
Inp_PVFBad | BOOL | Not Visible | Not Required | Input | Signal quality or communication status for input F 1 = Bad, 0 = OK. Default is false. |
Inp_PVFUncertain | BOOL | Not Visible | Not Required | Input | Signal quality for input F, 1 = Uncertain, 0 = OK. Default is false. |
Inp_SmartDvcFDiagAvailable | BOOL | Not Visible | Not Required | Input | 1 = SMART device on Inp_PVFData diagnostics available. Typically used to indicate device requires action to keep operating as expected. Default is false. |
Inp_PVGBad | BOOL | Not Visible | Not Required | Input | Signal quality or communication status for input G 1 = Bad, 0 = OK. Default is false. |
Inp_PVGUncertain | BOOL | Not Visible | Not Required | Input | Signal quality for input G, 1 = Uncertain, 0 = OK. Default is false. |
Inp_SmartDvcGDiagAvailable | BOOL | Not Visible | Not Required | Input | 1 = SMART device on Inp_PVGData diagnostics available. Typically used to indicate device requires action to keep operating as expected. Default is false. |
Inp_PVHBad | BOOL | Not Visible | Not Required | Input | Signal quality or communication status for input H 1 = Bad, 0 = OK. Default is false. |
Inp_PVHUncertain | BOOL | Not Visible | Not Required | Input | Signal quality for input H, 1 = Uncertain, 0 = OK. Default is false. |
Inp_SmartDvcHDiagAvailable | BOOL | Not Visible | Not Required | Input | 1 = SMART device on Inp_PVHData diagnostics available. Typically used to indicate device requires action to keep operating as expected. Default is false. |
Cfg_AllowDisable | BOOL | Not Visible | Not Required | Input | 1 = Allow maintenance to disable alarms. Default is true. |
Cfg_AllowShelve | BOOL | Not Visible | Not Required | Input | 1 = Allow operator to shelve alarms. Default is true. |
Cfg_HasPVA | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVAData is connected in logic. Default is true. |
Cfg_HasPVB | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVBData is connected in logic. Default is true. |
Cfg_HasPVC | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVCData is connected in logic. Default is true. |
Cfg_HasPVD | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVDData is connected in logic. Default is false. |
Cfg_HasPVE | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVEData is connected in logic. Default is false. |
Cfg_HasPVF | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVFData is connected in logic. Default is false. |
Cfg_HasPVG | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVGData is connected in logic. Default is false. |
Cfg_HasPVH | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVHData is connected in logic. Default is false. |
Cfg_UsePVA | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVAData should be used in PV calculation if good. Default is true. |
Cfg_UsePVB | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVBData should be used in PV calculation if good. Default is true. |
Cfg_UsePVC | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVCData should be used in PV calculation if good. Default is true. |
Cfg_UsePVD | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVDData should be used in PV calculation if good. Default is false. |
Cfg_UsePVE | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVEData should be used in PV calculation if good. Default is false. |
Cfg_UsePVF | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVFData should be used in PV calculation if good. Default is false. |
Cfg_UsePVG | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVGData should be used in PV calculation if good. Default is false. |
Cfg_UsePVH | BOOL | Not Visible | Not Required | Input | 1 = Inp_PVHData should be used in PV calculation if good. Default is false. |
Cfg_RejectUncertain | BOOL | Not Visible | Not Required | Input | 1 = Reject an input if its quality is uncertain. Default is false. |
Cfg_UseStdDev | BOOL | Not Visible | Not Required | Input | 1 = Reject outside tau standard deviations; 0 = Reject ouside Cfg_AbsDev from mean. Default is false. |
Cfg_CalcAvg | BOOL | Not Visible | Not Required | Input | 1 = Calculate average of good inputs; 0 = calculate median of good inputs. Default is false. |
Cfg_UseInpSrcQPVA | BOOL | Not Visible | Not Required | Input | 1 = Use PVA SrcQ input for rejection decisions. Default is false. |
Cfg_UseInpSrcQPVB | BOOL | Not Visible | Not Required | Input | 1 = Use PVB SrcQ input for rejection decisions. Default is false. |
Cfg_UseInpSrcQPVC | BOOL | Not Visible | Not Required | Input | 1 = Use PVC SrcQ input for rejection decisions. Default is false. |
Cfg_UseInpSrcQPVD | BOOL | Not Visible | Not Required | Input | 1 = Use PVD SrcQ input for rejection decisions. Default is false. |
Cfg_UseInpSrcQPVE | BOOL | Not Visible | Not Required | Input | 1 = Use PVE SrcQ input for rejection decisions. Default is false. |
Cfg_UseInpSrcQPVF | BOOL | Not Visible | Not Required | Input | 1 = Use PVF SrcQ input for rejection decisions. Default is false. |
Cfg_UseInpSrcQPVG | BOOL | Not Visible | Not Required | Input | 1 = Use PVG SrcQ input for rejection decisions. Default is false. |
Cfg_UseInpSrcQPVH | BOOL | Not Visible | Not Required | Input | 1 = Use PVH SrcQ input for rejection decisions. Default is false. |
Cfg_HasPVNav | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI to enable navigation to a connected PV (Val) object. Default is false. |
Cfg_HasMoreObj | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI an object with more information is available. Default is false. |
Cfg_HasNav | SINT | Not Visible | Not Required | Input | Set bits indicate which navigation buttons are enabled .0=PVA, .1=PVB, ..., .7=PVH Default is 0. |
Cfg_MinGood | DINT | Not Visible | Not Required | Input | Minimum good inputs for good PV [1..number of "Cfg_Has" inputs]. Default is 2. |
Cfg_CalcWhen2 | DINT | Not Visible | Not Required | Input | PV calculation when only 2 good inputs: 0 = average, 1 = minimum, 2 = maximum. Default is 0. |
Cfg_PVEUMin | REAL | Not Visible | Not Required | Input | PV (Output) minimum for display PV units. Valid = any float. Default is 0.0. |
Cfg_PVEUMax | REAL | Not Visible | Not Required | Input | PV (Output) maximum for display PV units. Valid = any float. Default is 100.0. |
Cfg_AbsDevLim | REAL | Not Visible | Not Required | Input | Absolute deviation threshold for PV units. Valid = any nonnegative float: reject ouside this deviation from mean. Default is 10.0. |
Cfg_OoRHiLim | REAL | Not Visible | Not Required | Input | Out-of-range (fail) high limit for PV units. Valid = any float. Default is 103.958336. |
Cfg_OoRLoLim | REAL | Not Visible | Not Required | Input | Out-of-range (fail) low limit for PV units. Valid = any float. Default is -2.0833333. |
Cfg_OoRDB | REAL | Not Visible | Not Required | Input | Out-of-range (fail) deadbandfor PV units. Valid = any nonnegative float. Default is 0.41666666. |
Cfg_PVDecPlcs | SINT | Not Visible | Not Required | Input | Number of decimal places for PV display. Valid = 0,1,2,3,4,5,6. Default is 2. |
Cfg_CnfrmReqd | SINT | Not Visible | Not Required | Input | Operator Command Confirmation Required. Represents the type of command confirmation required. 0 = None, 1 = Command confirmation required, 2 = Performer e-signature required, 3 = Performer and approver e-signature required. Default is 0. |
PSet_Owner | DINT | Not Visible | Not Required | Input | Program owner request ID (non-zero) or release (zero) (Valid = any integer). Default is 0. |
PCmd_Reset | BOOL | Not Visible | Not Required | Input | Program command to reset all alarms requiring Reset. Default is false. |
XCmd_Reset | BOOL | Not Visible | Not Required | Input | External command to reset all alarms and latched shed conditions. The instruction clears this operand automatically. Default is false. |
XCmd_ResetAckAll | BOOL | Not Visible | Not Required | Input | External command to acknowledge and reset all alarms and latched shed conditions. The instruction clears this operand automatically. Default is false. |
Public Output Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
|---|---|---|---|---|---|
EnableOut | BOOL | Not Visible | Not Required | Output | Enable Output - System Defined Parameter |
Val | REAL | Visible | Not Required | Output | Selected analog PV (including substitute PV, if used) (PV units). |
Val_PVA | REAL | Visible | Not Required | Output | Analog value (actual) from input A (PV units). |
Val_PVB | REAL | Visible | Not Required | Output | Analog value (actual) from input B (PV units). |
Val_PVC | REAL | Visible | Not Required | Output | Analog value (actual) from input C (PV units). |
Val_PVD | REAL | Not Visible | Not Required | Output | Analog value (actual) from input D (PV units). |
Val_PVE | REAL | Not Visible | Not Required | Output | Analog value (actual) from input E (PV units). |
Val_PVF | REAL | Not Visible | Not Required | Output | Analog value (actual) from input F (PV units). |
Val_PVG | REAL | Not Visible | Not Required | Output | Analog value (actual) from input G (PV units). |
Val_PVH | REAL | Not Visible | Not Required | Output | Analog value (actual) from input H (PV units). |
Val_InpPV | REAL | Not Visible | Not Required | Output | Selected PV (PV units). |
Val_PVEUMin | REAL | Not Visible | Not Required | Output | Minimum of PV range = Min (Cfg_PVEUMin, Cfg_PVEUMax) (PV units). |
Val_PVEUMax | REAL | Not Visible | Not Required | Output | Maximum of PV range = Max (Cfg_PVEUMin, Cfg_PVEUMax) (PV units). |
Out_SmartDvcSts | DINT | Not Visible | Not Required | Output | Status code of a SMART device provided by Inp_SmartDvcASts or Inp_SmartDvcBSts or Inp_SmartDvcCSts or Inp_SmartDvcDSts or Inp_SmartDvcESts or Inp_SmartDvcFSts or Inp_SmartDvcGSts or Inp_SmartDvcHSts. Highest status code selected. |
Val_NumPVs | DINT | Not Visible | Not Required | Output | Number of PVs that are currently used in calculating Val_CalcPV. |
Sts_Initialized | BOOL | Not Visible | Not Required | Output | 1 = Instruction is initialized. Use Inp_InitializeReq to reinitialize. |
Sts_SmartDvcDiagAvailable | BOOL | Not Visible | Not Required | Output | 1 = Diagnostics of a SMART device is currently available. Typically used to indicate one of the devices requires action to keep operating as expected. |
Sts_PVBad | BOOL | Not Visible | Not Required | Output | 1 = At least one input channel PV is bad quality or out of range. |
Sts_PVUncertain | BOOL | Not Visible | Not Required | Output | 1 = At least one input channel PV value is uncertain quality. |
Sts_PVAReject | BOOL | Visible | Not Required | Output | 1 = Input A rejected, not used to calculate PV. |
Sts_PVBReject | BOOL | Visible | Not Required | Output | 1 = Input B rejected, not used to calculate PV. |
Sts_PVCReject | BOOL | Visible | Not Required | Output | 1 = Input C rejected, not used to calculate PV. |
Sts_PVDReject | BOOL | Not Visible | Not Required | Output | 1 = Input D rejected, not used to calculate PV. |
Sts_PVEReject | BOOL | Not Visible | Not Required | Output | 1 = Input E rejected, not used to calculate PV. |
Sts_PVFReject | BOOL | Not Visible | Not Required | Output | 1 = Input F rejected, not used to calculate PV. |
Sts_PVGReject | BOOL | Not Visible | Not Required | Output | 1 = Input G rejected, not used to calculate PV. |
Sts_PVHReject | BOOL | Not Visible | Not Required | Output | 1 = Input H rejected, not used to calculate PV. |
SrcQ_IOA | SINT | Not Visible | Not Required | Output | Source and quality of Input A (enumeration). |
SrcQ_IOB | SINT | Not Visible | Not Required | Output | Source and quality of Input B (enumeration). |
SrcQ_IOC | SINT | Not Visible | Not Required | Output | Source and quality of Input C (enumeration). |
SrcQ_IOD | SINT | Not Visible | Not Required | Output | Source and quality of Input D (enumeration). |
SrcQ_IOE | SINT | Not Visible | Not Required | Output | Source and quality of Input E (enumeration). |
SrcQ_IOF | SINT | Not Visible | Not Required | Output | Source and quality of Input F (enumeration). |
SrcQ_IOG | SINT | Not Visible | Not Required | Output | Source and quality of Input G (enumeration). |
SrcQ_IOH | SINT | Not Visible | Not Required | Output | Source and quality of Input H (enumeration). |
SrcQ_IO | SINT | Not Visible | Not Required | Output | Source and quality of calculated PV (enumeration). |
SrcQ | SINT | Not Visible | Not Required | Output | Source and quality of primary Val/Sts (enumeration). |
Sts_eSts | SINT | Not Visible | Not Required | Output | Device confirmed status (enum): 0 = PV Good, 1: PV Uncertain, 2: PV Bad. |
Sts_eFault | INT | Not Visible | Not Required | Output | Device fault status (enum): 0 = None, 17 = Any Reject, 18 = Min Good, 32 = Fail, 34 = Bad Config. |
Sts_eNotify | SINT | Not Visible | Not Required | Output | All alarm status enumerated values: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_eNotifyAll | SINT | Not Visible | Not Required | Output | All alarm status enumerated values including related objects: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_eNotifyAnyReject | SINT | Not Visible | Not Required | Output | Any Reject alarm status enumerated values: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_eNotifyMinGood | SINT | Not Visible | Not Required | Output | Min Good alarm status enumerated values: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_eNotifyFail | SINT | Not Visible | Not Required | Output | Fail alarm status enumerated values: 0 = Not in alarm, acknowledged, 1 = Not in alarm, unacknowledged or reset required, 2 = Low severity alarm, acknowledged, 3 = Low severity alarm, unacknowledged, 4 = Medium severity alarm, acknowledged, 5 = Medium severity alarm, unacknowledged, 6 = High severity alarm, acknowledged, 7 = High severity alarm, unacknowledged, 8 = Urgent severity alarm, acknowledged, 9 = Urgent severity alarm, unacknowledged. |
Sts_UnackAlmCount | DINT | Not Visible | Not Required | Output | Count of unacknowledged alarms. |
Sts_MaintByp | BOOL | Not Visible | Not Required | Output | 1 = Device has a maintenance bypass function active. |
Sts_Err | BOOL | Visible | Not Required | Output | 1 = Error in config, see detail bits for reason. |
Sts_ErrEU | BOOL | Not Visible | Not Required | Output | 1 = Error in config: Cfg_PVEUMax cannot equal Cfg_PVEUMin. |
Sts_ErrHas | BOOL | Not Visible | Not Required | Output | 1 = Error in config: at least one Cfg_HasPVx must be 1. |
Sts_ErrUse | BOOL | Not Visible | Not Required | Output | 1 = Error in config: at least one Cfg_UsePVx must be 1. |
Sts_ErrMinGood | BOOL | Not Visible | Not Required | Output | 1 = Error in config: Cfg_MinGood must be in the range [1..8]. |
Sts_ErrOoRDB | BOOL | Not Visible | Not Required | Output | 1 = Error in configuration: Cfg_OoRDB deadband is < 0.0. |
Sts_ErrAlm | BOOL | Not Visible | Not Required | Output | 1 = Error in logix tag-based alarm settings. |
Sts_Alm | BOOL | Not Visible | Not Required | Output | 1 = An alarm is active. |
Sts_AlmInh | BOOL | Not Visible | Not Required | Output | 1 = An alarm is shelved, disabled or suppressed: display icon. |
Sts_AnyReject | BOOL | Not Visible | Not Required | Output | 1 = At least one input has been rejected. |
Sts_MinGood | BOOL | Not Visible | Not Required | Output | 1 = At minimum required number of good inputs, next reject/fail will result in bad PV. |
Sts_Fail | BOOL | Not Visible | Not Required | Output | 1 = Total signal failure (too many inputs rejected). |
Sts_RdyAck | BOOL | Not Visible | Not Required | Output | 1 = An alarm is ready to be acknowledged. |
Sts_RdyReset | BOOL | Not Visible | Not Required | Output | 1 = A latched alarm or shed condition is ready to be reset. |
XRdy_Reset | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_Reset, enable HMI button. |
XRdy_ResetAckAll | BOOL | Not Visible | Not Required | Output | 1 = Ready for XCmd_ResetAckAll, enable HMI button. |
Val_Owner | DINT | Not Visible | Not Required | Output | Current object owner ID (0 = not owned). |
Private Input Members | Data Type | Description |
|---|---|---|
OCmd_Reset | BOOL | Operator command to reset all alarms requiring reset. Default is false. |
OCmd_ResetAckAll | BOOL | Operator command to reset and acknowledge all alarms. Default is false. |
Private Output Members | Data Type | Description |
|---|---|---|
HMI_BusObjIndex | DINT | HMI bus object index. Default is 0. |
ORdy_Reset | BOOL | 1 = Ready for OCmd_Reset (enables HMI button). |
ORdy_ResetAckAll | BOOL | 1 = Ready for OCmd_ResetAckAll (enables HMI button). |
Public InOut Members | Data Type | Description |
|---|---|---|
BusObj | BUS_OBJ | Bus component |
Public InOut Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
|---|---|---|---|---|---|
BusObj | BUS_OBJ | Visible | Required | InOut | Bus component |
BUS_OBJ Structure
Members | Data Type | Description |
|---|---|---|
Inp_Cmd | DINT | Input to assert commands |
Out_Cmd | DINT | Resultant commands |
Inp_CmdLLH | DINT | Input for level normally high commands |
Out_CmdLLH | DINT | Resultant line level high commands |
Inp_Sts | DINT | Input to assert status |
Out_Sts | DINT | Resultant status |
Inp_CmdAck | DINT | Input to assert a command acknowledgment |
Out_CmdAck | DINT | Resultant command acknowledgments |
Inp_SeverityMax | DINT | Input: maximum alarm severity |
Out_SeverityMax | DINT | Resultant of maximum alarm severity |
Cfg_CmdMask | DINT | Propagation mask for commands |
Cfg_CmdLLHMask | DINT | Propagation mask for line level high commands |
Cfg_StsMask | DINT | Propagation mask for status |
Ref_Index | DINT | Bus array index |
Alarms
Discrete tag-based alarms are defined for these members.
Member | Alarm name | Description |
|---|---|---|
Sts_Fail | Alm_Fail | Raised when the two sensor PVs are bad or out of range. |
Sts_AnyReject | Alm_AnyReject | Raised when any inputs configured to be used are rejected. |
Sts_MinGood | Alm_MinGood | Raised when the number of unrejected input is equal to the minimum number required to be good, meaning the next input failure results in a PV failure. |
Mark the alarm as used or unused and set standard configuration members of the discrete tag-based alarm. Access alarm elements using this format:
PAIMTag.@Alarms.AlarmName.AlarmElement
There are Program, Operator, and External commands that enable the Reset and Reset & Acknowledge of all alarms of the instruction (Alarm Set) at the same time. This diagram shows how the commands interact with the PAIM instruction.

Operation
This diagram illustrates the functionality of the PAIM instruction:

Initialization
The instruction is normally initialized in the instruction first run. Request re-initialization by setting Inp_InitializeReq = 1. For proper initialization, when adding the instruction while performing an online edit of the code, make sure that Inp_InitializeReq = 1, the default value.
Configuration of Strings for HMI
Configure strings for HMI faceplates, as seen in
FactoryTalk View
, and for the Logix Designer
configuration dialog box. The strings are set to extended properties of tag items. Configure the strings in Logix Designer
only.- Description
- Label for graphic symbol
- Display Library for HMI Faceplate call-up
- Instruction name
- Area name
- URL link
- More Information
- Selected Analog PV engineering units – Units of Val member, Val.@Units.
- Analog input A description – Description of Inp_PVAData member, Inp_PVAData.@Label.
- Analog input B description – Description of Inp_PVBData member, Inp_PVBData.@Label
- Analog input C description – Description of Inp_PVCData member, Inp_PVCData.@Label.
- Analog input D description – Description of Inp_PVDData member, Inp_PVDData.@Label.
- Analog input E description – Description of Inp_PVEData member, Inp_PVEData.@Label.
- Analog input F description – Description of Inp_PVFData member, Inp_PVFData.@Label.
- Analog input G description – Description of Inp_PVGData member, Inp_PVGData.@Label.
- Analog input H description – Description of Inp_PVHData member, Inp_PVHData.@Label.
- Analog input A navigation – Navigation metadata of Inp_PVAData member.
- Analog input B navigation – Navigation metadata of Inp_PVBData member.
- Analog input C navigation – Navigation metadata of Inp_PVCData member.
- Analog input D navigation – Navigation metadata of Inp_PVDData member.
- Analog input E navigation – Navigation metadata of Inp_PVEData member.
- Analog input F navigation – Navigation metadata of Inp_PVFData member.
- Analog input G navigation – Navigation metadata of Inp_PVGData member.
- Analog input H navigation – Navigation metadata of Inp_PVHData member.
Monitor the PAIM Instruction
Use the operator faceplate from the PlantPAx library of Process objects for monitoring.
Affects Math Status Flags
No.
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
|---|---|
Prescan | Rung-condition-out clears to false. |
Instruction first run | All commands that are automatically cleared on each execution are cleared and ignored. PSet_Owner and Val_Owner are set to 0. Ensure the constants for the Thompson Tau test logic have not been zeroed out. The instruction executes normally. |
Rung-condition-in is false | Rung-condition-out is cleared to false. All commands that are automatically cleared on each execution are cleared and ignored. PSet_Owner and Val_Owner are set to 0. Latched alarms are reset. Clear Bus Object commands and HMI Bus Object Index Execute Bus command on receipt for Disable, Enable, Suppress, Unsuppress all alarms. Execute Bus command status propagation. Internal timers are reset. |
Rung-condition-in is true | Set rung-condition-out to rung-condition-in. The instruction executes. |
Postscan | Rung-condition-out is cleared to false. |
Function Block Diagram
Condition/State | Action Taken |
|---|---|
Prescan | EnableOut is cleared to false. |
Instruction first run | All commands that are automatically cleared on each execution are cleared and ignored. PSet_Owner and Val_Owner are set to 0. Ensure the constants for the Thompson Tau test logic have not been zeroed out. The instruction executes normally. |
Instruction first scan | See Instruction first run in the Function Block Diagram table. |
EnableIn is false | EnableOut is cleared to false. All commands that are automatically cleared on each execution are cleared and ignored. PSet_Owner and Val_Owner are set to 0. Latched alarms are reset. Clear Bus Object commands and HMI Bus Object Index Execute Bus command on receipt for Disable, Enable, Suppress, Unsuppress all alarms. Execute Bus command status propagation. Internal timers are reset. |
EnableIn is true | EnableOut is set to true. The instruction executes. |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
In Structured Text, EnableIn is always true during normal scan. The instruction executes when it is in the control path activated by the logic.
Condition/State | Action Taken |
|---|---|
Prescan | See Prescan in the Function Block Diagram table. |
Instruction first run | See Instruction first run in the Function Block Diagram table. |
EnableIn is true | See EnableIn is true in the Function Block Diagram table. |
Postscan | See Postscan in the Function Block Diagram table. |
Example
The example uses the PAIM instruction to monitor one analog Process Variable (PV) by using up to eight analog input signals (sensors, transmitters). The PAIM instruction allows you to display a temperature, pressure, level, or other PV on a user interface or use the PV in control logic, and the following apply:
- Have three or more sensors for that PV, for example, six thermocouples.
- Calculate a PV with the mean or median of the sensor input values.
The example uses the PAIM instruction to average multiple sensors for a single PV. In this example, an application uses three analog sensors (A, B, C). The average of these analogs is used elsewhere in logic to control a separate application element.
The Inp_PVAData, Inp_PVBData, and Inp_PVCData parameters are connected to the values from the three analog transmitters. The fault status of each sensor is tied to the bad input of the PAIM (for example, Inp_PVABad). The output parameters Val, Sts_PVBad and Sts_PVUncertain, can then be connected to the Inp_PVData, Inp_PVUncertain and Inp_ChanFault for control.
Ladder Diagram

Function Block Diagram

Structured Text
PAI(AIT_301A);
PAI(AIT_301B);
PAI(AIT_301C);
AY_301.Inp_PVAData := AIT_301A.Val;
AY_301.Inp_PVASrcQ := AIT_301A.SrcQ;
AY_301.Inp_PVANotify := AIT_301A.Sts_eNotify;
AY_301.Inp_PVBData := AIT_301B.Val;
AY_301.Inp_PVBSrcQ := AIT_301B.SrcQ;
AY_301.Inp_PVBNotify := AIT_301B.Sts_eNotify;
AY_301.Inp_PVCData := AIT_301C.Val;
AY_301.Inp_PVCSrcQ := AIT_301C.SrcQ;
AY_301.Inp_PVCNotify := AIT_301C.Sts_eNotify;
PAIM(AY_301);
AI_301.Inp_PVData := AY_301.Val;
AI_301.Inp_ChanFault := AY_301.Sts_PVBad;
AI_301.Inp_PVUncertain := AY_301.Sts_PVUncertain;
PAI(AI_301);
Provide Feedback