Bit Field Distribute with Target (BTDT)
This information applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers. Controller differences are noted where applicable.
The BTDT instruction first copies the Target to the Destination. Then the instruction copies the specified bits from the Source, shifts the bits to the appropriate position, and writes the bits into the Destination. The Target and Source remain unchanged.
Available Languages
Ladder Diagram
This instruction is not available in a ladder diagram.
Function Block

Structured Text
BTDT(BTDT_tag);
Operands
Function Block
Operand | Type | Format | Description |
|---|---|---|---|
BTDT tag | FBD_BIT_FIELD_DISTRIBUTE | structure | BTDT structure |
Structured Text
Input Parameter | Data Type | Description |
|---|---|---|
EnableIn | BOOL | If cleared, the instruction does not execute and outputs are not updated. If set, the instruction executes.
Default is set. |
Source | DINT | Input value containing the bits to move to Destination.
Valid = any integer |
SourceBit | DINT | The bit position in Source (lowest bit number from where to start the move).
Valid = 0-31 |
Length | DINT | Number of bits to move.
Valid = 1-32 |
DestBit | DINT | The bit position in Dest (lowest bit number to start copying bits into).
Valid = 0-31 |
Target | DINT | Input value to move to Dest prior to moving bits from the Source.
Valid = any integer |
Output Parameter | Data Type | Description |
|---|---|---|
EnableOut | BOOL | Indicates if instruction is enabled. |
Dest | DINT | Result of the bit move operation. |
See
Structured Text Syntax
for information on the syntax of expressions within structured text.Description
When true, the BTDT instruction first copies the Target to the Destination, and copies a group of bits from the Source to the Destination. The group of bits is identified by the Source bit (lowest bit number of the group) and the Length (number of bits to copy). The Destination bit identifies the lowest bit number bit to start with in the Destination. The Source and Target remains unchanged.
If the length of the bit field extends beyond the Destination, the instruction does not save the extra bits. Any extra bits do not wrap to the next word.
Affects Math Status Flags
Controllers | Affected Math Status Flag |
|---|---|
CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Yes |
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | No |
See Math Status Flags.
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Function Block
Condition/State | Action Taken |
|---|---|
Prescan | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is false | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is true | EnableIn and EnableOut bits are set to true. The instruction executes. |
Instruction first run | N/A |
Instruction first scan | N/A |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
Condition/State | Action Taken |
|---|---|
Prescan | See Prescan in the Function Block table. |
Normal Execution | See Tag.EnableIn is true in the Function Block table. |
Postscan | See Postscan in the Function Block table. |
Example
Step 1
The controller copies Target into Dest.

Step 2
The SourceBit and the Length specify which bits in Source to copy into Dest. Starting at DestBit, Source and Target remain unchanged.

Function Block

Structured Text
BTDT_01.Source := sourceSTX;
BTDT_01.SourceBit := source_bitSTX;
BTDT_01.Length := LengthSTX;
BTDT_01.DestBit := dest_bitSTX;
BTDT_01.Target := TargetSTX;
BTDT(BTDT_01);
distributed_value := BTDT_01.Dest;
Provide Feedback