Crankshaft Position Monitor (CPM)
This instruction applies to the Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, and GuardLogix 5580 controllers.
The Crankshaft Position Monitor instruction is used to determine the slide position of the press by monitoring the Brake (BCAM), Dynamic (DCAM), and Takeover (TCAM) cams and representing the position as Top, Down, or Up by using the Slide Zone output. Also, the Top Zone, Down Zone, and Up Zone Boolean outputs are provided for monitoring and diagnostic purposes.
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
WARNING:
This instruction is specified with the intent that the Slide Zone output is used to source the Slide Zone input of the Clutch Brake Inch Mode (CBIM), Clutch Brake Single Stroke Mode (CBSSM), Clutch Brake Continuous Mode (CBCM), and Camshaft Monitor (CSM) instructions.
Normal stop operation of a press begins when the slide enters the Top zone. A successful stop occurs when the press stops in the Top zone. During normal stopping, the speed of the press may cause the press to stop in the Down zone. This is called an overrun. To minimize this, the DCAM can be enabled to generate an early Top zone, allowing the press to begin stopping early.
WARNING:
When required, the DCAM should only be enabled for normal stopping, based on speed of the press. Do not adjust the DCAM to account for deteriorating brake performance.
WARNING:
WARNING:
Reversing the press should only be performed during set up mode by using the Clutch Brake Inch Mode (CBIM) instruction. Reversing the press is only permitted for moving the slide from the Down zone to the Top zone where the CBIM instruction automatically stops the press at Top. A fault occurs when reverse movement continues into the Up zone.Operands
IMPORTANT:
Do not use the same tag name for more than one instruction in the same program. Do not write to any instruction output tag under any circumstances.
WARNING:
If you change instruction parameters while in Run mode, you must accept the pending edits and cycle the controller mode from Program to Run for the changes to take effect.
The following table provides the parameters used to configure the instruction. These parameters cannot be changed at runtime.
Operand | Data Type | Description |
|---|---|---|
CPM | CB_CRANKSHAFT_POSITION_MONITOR | This parameter is a backing tag that maintains important execution information for each usage of this instruction. ATTENTION: To avoid unexpected operation do not reuse this backing tag and its members. Do not write to any of the tag members anywhere else in the program. |
Cam Profile | BOOL | This parameter determines the cam profile used to generate the Slide Zone values. A (0) - See CPM – Cam Profiles and CPM – Normal Operation with Cam Profile A below. B (1) - See CPM – Cam Profiles and CPM – Normal Operation with Cam Profile B below. |
The following table explains the instruction inputs. The inputs may be field device signals from input devices or derived from user logic.
Operand | Data Type | Description | |
|---|---|---|---|
Enable | BOOL | This signal is used to enable the Crankshaft Position Monitor (CPM) instruction. ON (1): The instruction outputs are enabled. OFF (0): The instruction outputs are disabled. | |
Brake Cam (BCAM) | BOOL | This input is sourced by the cam monitoring device (hard cam) or application logic (soft cam). | |
Cam Profile A | This input specifies the overrun point and the Top zone when dynamic stopping is disabled. OFF (0) -> ON (1): While the press is running and dynamic stopping is disabled, this transition signals the end of the Up zone and the start of the Top zone. ON (1) -> OFF (0): While the press is stopping, this transition causes the Camshaft Monitor instruction to generate a brake fault. | ||
Cam Profile B | This input specifies the overrun point and the zone where immediate braking of the press is allowed. OFF (0) - No effect. OFF (0) -> ON (1): When detected while the press is stopping, this transition causes the Camshaft Monitor (CSM) instruction to generate a brake fault. While the press is running, this transition signals the end of the Top zone and start of the Down zone. ON (1) -> OFF (0): While the press is running, this transition must occur after the OFF (0) to ON (1) transition of the Takeover cam (TCAM). | ||
Takeover Cam (TCAM) | BOOL | This input is sourced by the cam monitoring device (hard cam) or application logic (soft cam). | |
Cam Profile A | This input is used to indicate the start of the Up zone. OFF (0) -> ON (1): This transition signals the start of the end of the Down zone and the start of the Up zone. ON (1) -> OFF (0: When dynamic stopping is enabled, this transition has no effect unless the dynamic stop signal has yet to occur. When this happens, this transition signals the end of the Up zone and start of the Top zone. | ||
Cam Profile B | This input is used to indicate the start of the Up zone. OFF (0): The press is considered to be in the Down zone when the Brake cam (BCAM) is ON (1). OFF (0) -> ON (1): This transition signals the start of the Up zone and the end of the Down zone and must occur before the ON (1) to OFF (0) transition of the BCAM. ON (1) -> OFF (0): When dynamic stopping is not enabled, this transition signals the end of the upstroke and the start of the Top zone. When dynamic stopping is enabled, this transition has no effect unless the dynamic stop signal has yet to occur. In this case, the dynamic stopping enable behavior is performed. | ||
Dynamic Cam (DCAM) | BOOL | This input is used to generate an early top signal for fast-running presses. This input is sourced by a cam monitoring device (hard cam) or application logic (soft cam). This parameter is not safety-related. | |
Cam Profile A | When dynamic stopping is not required, this input should be sourced by the inverse of the Brake Cam (BCAM). OFF (0) -> ON (1): Dynamic stopping is enabled when this transition occurs at or after the ON (1) to OFF (0) transition of the BCAM. ON (1) -> OFF (0): This transition signals the end of upstroke and the start of the Top zone when it occurs before the OFF (0) to ON (1) transition of the Takeover cam (TCAM). | ||
Cam Profile B | When dynamic stopping is not required, this input should be sourced by the Takeover Cam (TCAM). OFF (0) -> ON (1): Dynamic stopping is enabled when this transition occurs at or after the OFF (0) to ON (1) transition of the TCAM. ON (1) -> OFF (0): This transition signals the end of Up zone and the start of the Top zone when it occurs at or before the ON (1) to OFF (0) transition of the TCAM. | ||
Input Status | BOOL | This input represents the combined status of the cam monitoring functions in addition to the I/O module status. ON: Inputs are valid. The Slide Zone status bit is set to 1. OFF: Inputs are invalid. All outputs are set to their de-energized or OFF (0) state. The Slide Zone status bit is set to 0. | |
Reverse | BOOL | Reversing the press should only be performed during set up mode by using the Clutch Brake Inch Mode (CBIM) instruction. Reversing the press is only permitted to move the slide from the Down zone to the Top zone where the Clutch Brake Inch Mode (CBIM) instruction automatically stops the press. A fault is generated when reverse movement is continued into the Up zone. OFF (0): Reverse operation is disabled. ON (1): When the slide is in the Down zone, this instruction lets the press move toward the Top zone. A fault is generated if this input is
ON (1) when the slide is in the Up zone. | |
Press Motion Status | BOOL | This input represents the motion status of the press and is sourced by Output 1 of the Main Valve Control (MVC) instruction or other valve control application logic. OFF (0): The press has stopped or a stop request has been issued. ON (1): The press is running or a start request has been issued. Important: When the press has been requested to stop at Top, overrun monitoring is enabled when the slide transitions from the Up to the Top zone. An overrun fault occurs when the slide continues to move into the Down zone. | |
Reset (1) | BOOL | This input clears the instruction faults provided the fault condition is not present. OFF (0) -> ON (1): The Fault Present and Fault Code outputs are reset. | |
(1)
ISO 13849-1 stipulates instruction reset functions must occur on falling edge signals. To comply with ISO 13849-1 requirements, add this logic immediately before this instruction. Rename the “Reset_Signal” tag in this example to your reset signal tagname. Then use the OSF instruction Output Bit tag as the instruction’s reset source.
The following table explains the instruction outputs. The outputs may be field device signals or derived from user logic.
Operand | Data Type | Description | ||||
|---|---|---|---|---|---|---|
Slide Zone | DINT | This output represents the position of the slide and the position information status. This output is used to source the Slide Zone input of the Clutch Brake Inch Mode (CBIM), Clutch Brake Single Stroke Mode (CBSSM), Clutch Brake Continuous Mode (CBCM), and Camshaft Monitor (CSM) instructions. This is a bit-mapped value where: Bit 0: Status OFF (0) - The Slide Zone information is invalid. Prevents the energizing of Output 1 on an initial start or immediately de-energized Output 1. ON (1) - Slide Zone information is valid. Bits 1 and 2: Slide Zone The following table lists how Bits 0 through 2 are used to represent the valid slide zones. | ||||
Bit 2 | Bit 1 | Bit 0 | Slide Zone | Decimal Value | ||
0 | 0 | 1 | Down | 1 | ||
0 | 1 | 1 | Up | 3 | ||
1 | 0 | 1 | Top | 5 | ||
Bits 3 through 31: Unused; Set to 0. | ||||||
Top Zone (TZ) | BOOL | This information bit indicates when the slide is in the Top zone. | ||||
Down Zone (DZ) | BOOL | This information bit indicates when the slide is in the Down zone. | ||||
Up Zone (UZ) | BOOL | This information bit indicates when the slide is in the Up zone. | ||||
Diagnostic Code | DINT | This output indicates the diagnostic status of the instruction. See the CPM – Diagnostic Codes below for a list of diagnostic codes. This parameter is not safety-related. | ||||
Fault Code | DINT | This output indicates the type of fault that occurred. See the CPM – Fault Codes below for a list of fault codes. This parameter is not safety-related. | ||||
Fault Present (FP) | BOOL | ON (1): A fault is present in the instruction. OFF (0): The instruction is operating normally. | ||||
IMPORTANT:
Do not write to any instruction output tag under any circumstances.
Cam Profiles
This instruction supports two cam profiles, A or B, selected by using the Cam Profile configurable parameter. The main difference between Cam Profiles A and B is the configuration of the Brake Cam (BCAM). In profile A, the BCAM is configured to represent the Top zone and in profile B, it is configured to represent the Down zone. The Takeover Cam (TCAM) in both profiles is configured to represent the Up zone.
These profile diagrams illustrate the relationships of the cams when the Dynamic Cam (DCAM) is enabled.
When enabled, the DCAM is configured the same way, with the ON (1) to OFF (0) transition during the Up zone generating the early Top zone. Depending upon the speed of the press, this transition can be configured to occur anytime during the Up zone. However, when the DCAM is disabled, it must be configured as follows:
- Profile A – The DCAM must be sourced by the inverse of the BCAM input source.
- Profile B – The DCAM must be sourced by the TCAM input source.

WARNING:
Cam angles are not shown in these cam profiles. The cam angles should be selected by qualified personnel.
WARNING:
When the Cam Profile is configured for A and dynamic stopping is disabled, the Dynamic Cam (DCAM) input must be sourced inverse of the Brake Cam (BCAM) input source.
WARNING:
When the Cam Profile is configured for B and dynamic stopping is disabled, the Dynamic Cam (DCAM) input must be sourced by the Takeover Cam (TCAM) input source.
Normal Operation with Cam Profile A
The following example describes normal operation when Cam Profile A is selected and the press is moving in the forward direction. The press starts with the slide at Top with the Takeover cam input (TCAM) OFF (0) and the Brake cam input (BCAM) ON (1) at (A) The Slide Zone is set to Top. As the press moves, the BCAM input transitions from ON (1) to OFF (0) at (B) and the Slide Zone changes from Top to Down. As the press continues moving, the TCAM input transitions from OFF (0) to ON (1) at (C) and the Slide Zone changes from Down to Up. Further press movement causes the Slide Zone output to change from Up to Top at different points depending on the Dynamic cam input (DCAM) configuration.
When the DCAM is enabled, the Slide Zone changes from Up to Top when the DCAM input transitions from ON (1) to OFF (0) while the TCAM input is ON (1) at (D). When the DCAM is disabled, the Slide Zone changes from Up to Top when the BCAM input transitions from OFF (0) to ON (1) at (D).

Normal Operation with Cam Profile B
The following example describes normal operation when Cam Profile B is selected and the press is moving in the forward direction. The press starts with slide at Top with Takeover cam input (TCAM) and Brake cam input (BCAM) OFF (0) at (A) and Slide Zone set to Top. As the press moves, the BCAM input transitions from OFF (0) to ON (1) at (B) and the Slide Zone changes from Top to Down. As the press continues moving, the TCAM input transitions from OFF (0) to ON (1) at (C) and Slide Zone changes from Down to Up. Further press movement causes the Slide Zone output to change from Up to Top at different points depending on the Dynamic cam input (DCAM) configuration.
When the DCAM is enabled, the Slide Zone output changes from Up to Top when the DCAM input transitions from ON (1) to OFF (0) while the TCAM input is ON (1) and the BCAM input is OFF (0) at (D). When the DCAM is disabled, the Slide Zone output changes from Up to Top when the TCAM input transitions ON (1) to OFF (0) at (D).

False Rung State Behavior
When the instruction is executed on a false rung, all instruction outputs are de-energized.
Fault Codes and Corrective Actions
The fault codes are listed in hexadecimal format followed by decimal format.
Fault Code | Description | Corrective Action | |
|---|---|---|---|
00 | No fault. | None. | |
16#20 32 | The Input Status input transitioned from ON (1) to OFF (0) while the instruction was executing. |
| |
16#1000 4096 | While the press was moving forward, slide movement from the Top zone to the Up zone was detected. |
| |
16#1001 4097 | While the press was moving forward, slide movement from the Down zone to the Top zone was detected. | ||
16#1002 4098 | While the press was moving forward, slide movement from the Up zone to the Down zone was detected. | ||
16#1003 4099 | While the press was moving forward, slide movement from the Up zone to the Down zone was detected. | ||
16#1004 4100 | Slide movement from the Top zone to the Down zone was detected while the press was reversing. Reverse movement is only permitted toward the Top zone. | ||
16#1005 4101 | Slide movement from the Down zone to the Up zone was detected while the press was reversing. Forward movement of the press is not permitted when Reverse is enabled. | ||
16#1006 4102 | The Dynamic cam (DCAM) is stuck OFF (0). |
| |
16#1007 4103 | The Dynamic cam (DCAM) is stuck ON (1). | ||
16#1008 4104 | Cam Profile A | The DCAM turned OFF (0) while the slide was in the Down zone. | |
Cam Profile B | N/A | ||
16#1009 4105 | Cam Profile A | The Takeover cam (TCAM) is stuck ON (0). |
|
Cam Profile B | N/A | ||
16#100A 4106 | Cam Profile A | N/A |
|
Cam Profile B | The Brake cam (BCAM) is stuck ON (0). | ||
16#1020 4128 | A request to reverse the press was made while the slide was in the Up zone. |
| |
16#1040 4160 | A slide overrun fault occurred. |
| |
Diagnostic Codes and Corrective Actions
The diagnostic codes are listed in hexadecimal format followed by decimal format
Fault Code | Description | Corrective Action |
|---|---|---|
00 | No fault. | None. |
16#20 32 | The Input Status input was OFF (0) when the instruction started. | Check the I/O module connection or the Camshaft Monitor (CSM) instruction used to source input status. Set the Input Status input to ON (1), if the inputs are not being sourced by a safety I/O module. |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Condition/State | Action Taken |
|---|---|
Prescan | Same as Rung-condition-in is false. |
Rung-condition-in is false | The .TZ, DZ, UZ, and FP is cleared to false. The Diagnostic Code, Fault Code, and Slide Code are set to 0. |
Rung-condition-in is true | The instruction executes as described in the Normal operation section. |
Postscan | Same as Rung-condition-in is false. |
Provide Feedback