Convert to BCD (TO_BCD)
This table lists the controllers and applications that support this instruction.
Architecture | Standard applications | Safety applications |
|---|---|---|
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes | No |
CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Yes | Yes |
The TO_BCD instruction converts a decimal value (0
Source
99,999,999) to a BCD value and stores the result in the Destination.
Source
99,999,999) to a BCD value and stores the result in the Destination.
TIP:
In Logix Designer version 36, the mnemonic for this instruction changed from TOD to TO_BCD.
Available Languages
Ladder Diagram

Function Block Diagram
Function Block Diagram supports these elements:
FBD Block

Structured Text
This instruction is not available in structured text.
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Ladder Diagram
Operand | Data Type CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Data Type CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Format | Description |
Source | SINT INT DINT | SINT INT DINT LINT USINT UINT UDINT ULINT | Immediate tag | Value to convert to BCD 0 Source 99,999,999 |
Destination | SINT INT DINT | SINT INT DINT LINT USINT UINT UDINT ULINT | tag | Tag to store the result |
Function Block Diagram
FBD Block
Operand | Type | Format | Description |
TO_BCD tag | FBD_CONVERT | Structure | TO_BCD structure |
FBD_CONVERT Structure
Input Member | Data Type | Description |
EnableIn | BOOL | Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set. |
Source | DINT | Input to the conversion instruction.
Valid = any integer |
Output Member | Data Type | Description |
EnableOut | BOOL | Enable output. |
Dest | DINT | Result of the conversion instruction. Math status flags are set for this output. |
Description
BCD is the Binary Coded Decimal number system that expresses individual decimal digits (0-9) in a 4-bit binary notation.
Source | Destination | Destination Type |
Negative source < 0 | 0 | |
Source > 9,999, 999,999, 999,999 | 16#9999_9999_9999_9999 | ULINT |
Source > 9,999, 999,999, 999,999 | 16#9999_9999_9999_9999 | LINT |
Source > 99,999,999 | 16#9999_9999 | UDINT |
Source > 99,999,999 | 16#9999_9999 | DINT |
Source > 99,999,999 | 16#9999 | UINT |
Source > 99,999,999 | 16#9999 | INT |
Source > 99,999,999 | 16#99 | USINT |
Source > 99,999,999 | 16#99 | SINT |
Affects Math Status Flags
Controllers | Affects Math Status Flags |
CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Conditional, see . |
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes |
Major/Minor Faults
See for operand related faults.
A minor fault will occur if: | Fault type | Fault code |
feature is enabled and overflow detected and Source < 0 | 4 | 4 |
feature is enabled and overflow detected and Source > 99,999,999 / 9,999, 999,999, 999,999 | 4 | 4 |
feature is enabled and overflow detected | 4 | 4 |
Execution
Ladder Diagram
Condition/State | Action Taken |
Prescan | N/A. |
Rung-condition-in is false | N/A. |
Rung-condition-in is true | The controller converts the Source to BCD and places the result in the Destination. |
Postscan | N/A. |
Function Block Diagram
FBD Block
Condition/State | Action Taken |
Prescan | N/A |
Tag.EnableIn is false. | EnableOut is cleared to false |
Tag.EnableIn is true | Dest = the result of computation in BCD value. If overflow occurs Clear EnableOut to false. else Set EnableOut to true. |
Instruction first scan | N/A |
Instruction first run | N/A |
Postscan | N/A |
Example
Ladder Diagram

Function Block

Provide Feedback
Source
99,999,999