D Flip-Flop (DFF)
This information applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram logic.
Function Block

Structured Text
DFF(DFF_tag);
Operands
Function Block
Operand | Type | Format | Description |
|---|---|---|---|
DFF tag | FLIP_FLOP_D | structure | DFF structure |
FLIP_FLOP_D Structure
Input Parameter | Data Type | Description |
|---|---|---|
EnableIn | BOOL | Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set. |
D | BOOL | The input to the instruction.
Default is cleared. |
Clear | BOOL | Clear input to the instruction. If set, the instruction clears Q and sets QNot. |
Clock | BOOL | Clock input to the instruction.
Default is cleared. |
Output Parameter | Data Type | Description |
|---|---|---|
EnableOut | BOOL | Indicates if instruction is enabled. |
Q | BOOL | The output of the instruction. |
QNot | BOOL | The complement of the Q output. |
Structured Text
Operand | Type | Format | Description |
|---|---|---|---|
DFF tag | FLIP_FLOP_D | structure | DFF structure |
See
Structured Text Syntax
for more information on the syntax of expressions within structured text.Description
When Clear is set, the instructions clears Q and sets QNot. Otherwise, if Clock is set and Clockn-1 is cleared, the instruction sets Q=D and sets QNot = NOT (D).
The instruction sets Clockn-1 = Clock state every scan.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See
Common Attributes
for operand-related faults.Execution
Function Block
Condition/State | Action Taken |
|---|---|
Prescan | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is false | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is true | EnableIn and EnableOut bits are set to true. The instruction executes. |
Instruction first run | Clockn-1 is set to 1.
Qn-1 is cleared to 0. |
Instruction first scan | Previous input Clock state is set True. Previous output Q state is set False. |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
Condition/State | Action Taken |
|---|---|
Prescan | See Prescan in the Function Block table. |
Normal Execution | See Tag.EnableIn is true in the Function Block table. |
Postscan | See Postscan in the Function Block table. |
Example
When Clock goes from cleared to set, the DFF instruction sets Q = D. When Clear is set, Q is cleared. The DFF instruction sets QNot to the opposite state of Q.
Function Block

Structured Text
DFF_03.D := d_input;
DFF_03.Clear := clear_input;
DFF_03.Clock := clock_input;
DFF(DFF_03);
q_output := DFF_03.Q;
qNot_output := DFF_03.QNot;
Provide Feedback