LINT data types
LINT data type is a 64-bit integer.
The LINT data type can be used in numerous instructions on
however the LINT data type cannot be used in most instructions on
.
Compact GuardLogix
5380, CompactLogix
5380, CompactLogix
5480, CompactLogix
5580, or GuardLogix
5580 controllerCompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570 controllersConsider the following when using LINT data type on
.
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570 controllersTip: | LINTs can only be used with copy (COP, CPS) instructions. They are used with the CST/WallClock Time attribute, time synchronization and Add-On Instructions. You cannot add, subtract, multiply, or divide this tag type. |
When using LINT data types, consider the following descriptions when these issues occur.
How to | Description |
|---|---|
Move/copy two double-integer DINT values into one LINT | Create a double integer array of two elements, total of 64 bits (that is, DINT[2], which can then be copied into one long integer. |
Correct Date/Time Display error | When a tag has a negative value, it cannot be displayed as Date/Time. In the tag editor, check whether the value is negative by changing the style of the tag from Date/Time to Binary. When the most significant bit (leftmost one) is 1, the value is negative and therefore cannot be displayed as a Date or Time. |
Provide Feedback