Motion Axis Home (MAH)
CompactLogix
5380, CompactLogix
5480, ControlLogix
5580, Compact GuardLogix
5380, and GuardLogix
5580 controllersUse the Motion Axis Home (MAH) instruction to home an axis. Two different homing modes can be selected during axis configuration: Active or Passive. If an Active homing sequence is selected, the axis executes the configured Home Sequence Type and establishes an absolute axis position. If Passive homing is selected, however, no specific homing sequence is executed and the axis is left waiting for the next marker pulse to establish the home position.
Architecture | Standard | Safety |
|---|---|---|
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes | No |
Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers | Yes | No |
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block
Structured Text
MAH(Axis,MotionControl);
Operands
Ladder Diagram and Structured Text
Operand | Type Tip: AXIS_CONSUMED is supported by Compact GuardLogix 5580, CompactLogix 5380, and CompactLogix 5480 controllers only. | Type Tip: AXIS_GENERIC is supported by the ControlLogix 5570 and the GuardLogix 5570 controllers only. | Format | Description |
|---|---|---|---|---|
Axis | AXIS_CIP_DRIVE AXIS_VIRTUAL | AXIS_CIP_DRIVE
AXIS_VIRTUAL
AXIS_GENERIC_DRIVE
AXIS_SERVO
AXIS_SERVO_DRIVE | Tag | Name of the axis on which to perform operation. For controllers that support the REF_TO motion data types, the supported axis operand type can be replaced by an equivalent REF_TO type. |
Motion Control | MOTION_INSTRUCTION | Tag | Structure used to access instruction status parameters. |
See Structured Text Syntax for more information on the syntax of expressions within structured text.
MOTION_INSTRUCTION Structure
Mnemonic | Description |
|---|---|
.EN (Enable) Bit 31 | It is set when the rung makes a false-to-true transition and remains set until the servo message transaction is completed and the rung goes false. |
.DN (Done) Bit 29 | It is set when axis home has been successfully completed or is aborted. |
.ER (Error) Bit 28 | It is set to indicate that the instruction detected an error, such as if you specified an unconfigured axis. |
.IP (In Process) Bit 27 | It is set on positive rung transition and cleared after the Motion Home Axis is complete, or terminated by a stop command, shutdown, or a servo fault. |
.PC (Process Complete) Bit 26 | It is set when axis home is successfully completed. |
Description
The MAH instruction is used to calibrate the absolute position of the specified axis. For axes that are configured as type Servo, the axis can be homed using Active, Passive, or Absolute Homing Mode configuration. For Feedback Only axes, only Passive and Absolute homing modes are available. Absolute Homing Mode requires the axis to be equipped with an absolute feedback device.
NOTE:
Absolute Homing mode is not available with a CIP axis. However, any successful Home sequence establishes an absolute position.
For CIP axes only, software overtravels are disabled if the Home status bit transitions to the FALSE state.
The MAH instructions sets the HomedStatus bit upon successful completion of the configured homing sequence. This bit indicates that an absolute machine reference position has been established. When this bit is set, operations that require a machine reference, such as Software Overtravel checking can be meaningfully enabled.
For non-CIP Drive axis data types, the HomedStatus bit is cleared under the following conditions:
- Download
- Control power cycle
- Reconnection to Motion Module
- Feedback Loss Fault
- Shutdown
Active Homing
When the axis Homing Mode is configured as Active, the physical axis is first activated for servo operation. As part of this process, all other motion in process is canceled and appropriate status bits are cleared. The axis is then homed using the configured Home Sequence, which may be Immediate, Switch, Marker, or Switch-Marker. The latter three Home Sequences result in the axis being jogged in the configured Home Direction and then, after the position is re-defined based on detection of the home event, the axis is automatically moved to the configured Home Position.
Passive Homing
When the axis Homing Mode is configured as Passive, the MAH instruction re-defines the actual position of a physical axis on the next occurrence of the encoder marker. Passive homing is most commonly used to calibrate Feedback Only axes to their markers, but can also be used on Servo axes. Passive homing is identical to active homing to an encoder marker, except that the motion controller does not command any axis motion.
After initiating passive homing, the axis must be moved past the encoder marker for the homing sequence to complete properly. For closed-loop Servo axes, this may be accomplished with a MAM or MAJ instruction. For physical Feedback Only axes, motion cannot be commanded directly by the motion controller, and must be accomplished via other means.
Absolute Homing
If the motion axis hardware supports an absolute feedback device, Absolute Homing Mode may be used. The only valid Home Sequence for an absolute Homing Mode is "immediate". In this case, the absolute homing process establishes the true absolute position of the axis by applying the configured Home Position to the reported position of the absolute feedback device. Prior to execution of the absolute homing process via the MAH instruction, the axis must be in the Axis Ready state with the servo loop disabled.
To successfully execute a MAH instruction on an axis configured for Active homing mode, the targeted axis must be configured as a Servo Axis Type. To successfully execute an MAH instruction, the targeted axis must be configured as either a Servo or Feedback Only axis. If any of these conditions are not met, the instruction errors.
NOTE:
The instruction execution may take multiple scans to execute because it requires multiple coarse updates to complete the request. The Done (.DN) bit is not set immediately, but only after the request is completed.
In this transitional instruction, the relay ladder, toggle the Rung-condition-in from cleared to set each time the instruction should execute.
Master Driven Speed Control (MDSC) and the MAH Instruction
When either an MDAC or MDCC is active:
- If a MAH is executed (goes IP) on a Master axis and the Master axis is not moving, the MDAC or MDCC remains active. If MDAC or MDCC is active while the MAH is executed (goes IP), the slave moves.
- If an MAH is executed (goes IP) on a Master axis and the Master axis is moving, the MAH will error. The MDAC or MDCC state remains unchanged.
- If an MAH is executed (goes IP) on a Slave axis and the Slave axis is not moving, the MDAC or MDCC is canceled.
- If an MAH is executed (goes IP) on a Slave axis while it is moving in MDSC Driven or Time Driven modes, the MAH will error. The state of MDAC or MDCC remains unchanged.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or a reference of incorrect type is passed to the Axis operand. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
|---|---|
Prescan | The .EN, .DN, .ER, and .IP bits are cleared to false. |
Rung-condition-in is false | The .EN bit is cleared to false if the .DN or .ER bit is true. |
Rung-condition-in is true | The .EN bit is set to true and the instruction executes. |
Postscan | N/A |
Structured Text
Condition/State | Action Taken |
|---|---|
Prescan | See Prescan in Ladder Diagram table |
Normal execution | See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table. |
Postscan | See Postscan in Ladder Diagram table. |
Error Codes
See Motion Error Codes (.ERR) for Motion Instructions.
Extended Error Codes
Extended Error Codes provide additional instruction specific information for the Error Codes that are generic to many instructions. See Motion Error Codes (.ERR) for Motion Instructions.
The following Extended Error codes help to pinpoint the problem when the MAH instruction receives a Servo Message Failure (12) error message or Illegal Homing Configuration (41).
Associated Error Code (decimal) | Extended Error Code (decimal) | Meaning |
|---|---|---|
SERVO_MESSAGE_FAILURE (12) | Process terminated on request (1) | Home execution followed by an instruction to shutdown/disable drive, or a motion stop instruction or a Processor change requests a cancel of Home. |
SERVO_MESSAGE_FAILURE (12) | No Resources (2) | Not enough memory resources to complete request. (SERCOS) |
SERVO_MESSAGE_FAILURE (12) | Object Mode conflict (12) | Axis is in shutdown. |
SERVO_MESSAGE_FAILURE (12) | Permission denied (15) | Enable input switch error. (SERCOS) |
SERVO_MESSAGE_FAILURE (12) | Device in wrong state (16) | Redefine Position, Home, and Registration 2 are mutually exclusive (SERCOS), device state not correct for action. (SERCOS) |
ILLEGAL_HOMING_CONFIG (41) | Home sequence (4) | The Home Sequence is incompatible with the Home Mode. |
ILLEGAL_HOMING_CONFIG (41) | Home speed of zero (6) | Home speed cannot be zero. |
ILLEGAL_HOMING_CONFIG (41) | Home return speed of zero (7) | The Home Return Speed cannot be zero. |
For the Error Code 54 – Maximum Deceleration Value is Zero, if the Extended Error returns a positive number (0-n) it is referring to the offending axis in the coordinate system. Go to the Coordinate System Properties General Tab and look under the Brackets ([ ])column of the Axis Grid to determine which axis has a Maximum Deceleration value of 0. Click on the ellipsis button next to the offending axis to access the Axis Properties screen. Go to the Dynamics tab and make the appropriate change to the Maximum Deceleration Value. If the Extended Error number is -1, this means the Coordinate System has a Maximum Deceleration Value of 0. Go to the Coordinate System Properties Dynamics Tab to correct the Maximum Deceleration value.
Status Bits
MAH Changes to Single Axis Status Bits
Bit Name | State | Meaning |
|---|---|---|
HomingStatus | TRUE | Axis is Homing. |
JogStatus | FALSE | Axis is no longer Jogging.* |
MoveStatus | FALSE | Axis is no longer Moving.* |
GearingStatus | FALSE | Axis is no longer Gearing. |
StoppingStatus | FALSE | Axis is no loner Stopping. |
*During portions of the active homing sequence these bits may be set and cleared. The MAH instruction uses the Move and Jog motion profile generators to move the axis during the homing sequence. This also means that any disruption in the Move or Jog motion profiles due to other motion instructions can affect the successful completion of the MAH initiated homing sequence.
If in Passive homing mode, the MAH instruction simply sets the Homing Status bit.
Provide Feedback