Equipment Sequence Override (SOVR)
This instruction applies to the
Logix Designer
5580 P-controllers. The Logix Designer
5580 P-controllers also support controller redundancy.
TIP:
When using this instruction with
ControlLogix
redundancy system, outputs controlled by this instruction may not be bumpless during redundancy switchover, if the instruction and sequence program are not scheduled in the highest priority task.
WARNING:
When using redundancy with an
Equipment Sequence
, sequence execution may not be as expected after switchover if the phase and sequence are not scheduled on the same task.Use the
Equipment Sequence
Override (SOVR) instruction to send a HOLD, STOP, or ABORT command to an Equipment Sequence
, regardless of ownership.
IMPORTANT:
The SOVR instruction is intended for emergencies only. Control Engineers should use caution when deciding to use it.
0
indicates that the SOVR instruction ran successfully. The other four codes indicate that the instruction did not run successfully and provide additional information about the reason for the instruction failure.This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
SOVR(SequenceName, Sequence Command, Result)
Operands
Ladder Diagram
Operand | Data Type | Format | Description |
Sequence Name | SEQUENCE | Name of the Equipment Sequence | Equipment Sequence to perform the command. |
Command | Command Enum | Name of the command | Command to send to the Equipment Sequence . Send one of these commands: HOLD, STOP, or ABORT |
Result | DINT | Tag | For an instruction to return a success or failure code, enter a DINT tag where the result code is to be stored. Otherwise, enter 0. |
Structured Text
The operands are the same as the Ladder Diagram.
Guidelines for using the SOVR Instruction
Guideline | Details |
|---|---|
Make sure you want to override other owners. | Under most circumstances, use the SCMD instruction to programmatically command an Equipment Sequence . However, use the SOVR instruction to command an Equipment Sequence under these conditions:
|
Limit execution of the SOVR instruction to a single scan. | Limit the execution of the SOVR instruction to a single scan. Each command applies to only a specific state or states. Once the Equipment Sequence changes state, the command is no longer valid. To limit execution, use methods such as:
|
Avoid making unnecessary command requests if the Equipment Sequence is generating sequence events. | Unnecessary command requests can flood the event processing buffers and cause you to miss significant events. |
SOVR Result Codes
Code (Desc) | Description |
|---|---|
0 | The command was successful. |
24579 | The caller is attached to this Sequence, but it is not the current Owner of it. A higher priority application is currently the Owner of this sequence. |
24582 | The caller already has override ownership of this Sequence. |
24583 | This sequence’s attachment table is full. |
24606 | The caller has already established an external attachment or override as a different owner type. |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index Through Arrays[1] for operand related faults.
Execution
At instruction execution, the SOVR instruction attempts to command the specified
Equipment Sequence
.Ladder Diagram
Condition | Action Taken |
|---|---|
Prescan | No action taken |
Rung-condition-in is false | No action taken |
Rung-condition-in is true | The instruction executes. |
Postscan | No action taken |
Structured Text
Condition | Action Taken |
|---|---|
Prescan | No action taken |
Rung-condition-in is false | No action taken |
Rung-condition-in is true | The instruction executes |
Postscan | No action taken |
Example
Ladder Diagram

Structured Text
if (OverrideControl) then
SOVR(Make_Product_101, Abort, Result);
end_if
Provide Feedback