Equipment Sequence Diagram instructions
The table describes the
Equipment Sequence
Diagram instructions. Icon | Icon Name | Description |
![]() | Add Step and Transition Pair | Use Add Step and Transition Pair to add a step and transition pair. Although added as a pair, you can select and edit each element separately. |
![]() | Add Disconnected Step | Use the Add Disconnected Step to add a step without adding a transition. |
![]() | Add Disconnected Transition | Use Add Disconnected Transition to add a transition without adding a step. |
![]() | Add Simultaneous Divergence | Use Add Simultaneous Divergence to create a branch where all linked steps execute simultaneously. |
![]() | Add Selective Divergence | Use Add Selective Divergence to create a divergence for a selective branch. In a selective divergence, only one of multiple paths is executed--the path containing the transition that first evaluates as TRUE. |
![]() | Add Simultaneous Convergence | Use Add Simultaneous Convergence to merge simultaneous execution paths back together. |
![]() | Add Selective Convergence | Use Add Selective Convergence ![]() |
Provide Feedback