Equipment Sequence Assign Sequence Identifier (SASI)
This instruction applies to the
Logix Designer
5580 P-controllers. The Logix Designer
5580 P-controllers also support controller redundancy.
TIP:
When using this instruction with
ControlLogix
redundancy system, outputs controlled by this instruction may not be bumpless during redundancy switchover, if the instruction and sequence program are not scheduled in the highest priority task.
WARNING:
When using redundancy with an
Equipment Sequence
, sequence execution may not be as expected after switchover if the phase and sequence are not scheduled on the same task.Use the Assign Sequence Identifier (SASI) instruction to assign a sequence ID to the
Equipment Sequence
. You can only set the sequence ID when these prerequisites are met:- The controller is online.
- TheEquipment Sequenceis in the IDLE state.
- You have taken ownership of theEquipment Sequence, or there is no other owner of theEquipment Sequence.
The sequence ID can be up to 82 characters in length, using these printable ASCII characters:
a-z, A-Z, 0-9, !"#$%&'()*+,-./:;<=>?@[\] ^_`{|}~ and space
This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
Ladder Diagram

Function Block Diagram
This instruction is not available in Function Block.
Structured Text
SASI(Sequence Name, Sequence Id, Result)
Operands
Ladder Diagram
Operand | Data Type | Format | Description |
Sequence Name | SEQUENCE | name of the Equipment Sequence | Equipment Sequence to which you want to assign an identifier. |
Sequence Id | STRING | Tag | Enter a STRING tag in which the identifier is stored, or a quoted string containing up to 82 characters. |
Result | DINT | Tag | For an instruction to return a success or failure code, enter a DINT tag where the result code is to be stored. Otherwise, enter 0. |
Structured Text
The operands are the same as for the Ladder Diagram.
SASI Result Codes
Code (Dec) | Description |
|---|---|
0 | the Sequence Id was successfully assigned. |
24578 | The Sequence state is not IDLE or there presently is a Sequence failure. |
24579 | Sequence is attached by another owner. |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index Through Arrays[1] for operand related faults.
Execution
At instruction execution, the SASI instruction attempts to assign a string identifier to the specified
Equipment Sequence
.Ladder Diagram
Condition | Action Taken |
|---|---|
Prescan | No action taken |
Rung-condition-in is false | No action taken |
Rung-condition-in is true | The instruction executes |
Postscan | No action taken |
Structured Text
Condition | Action Taken |
|---|---|
Prescan | No action taken |
Rung-condition-in is false | No action taken |
Rung-condition-in is true | The instruction executes |
Postscan | No action taken |
Example
Ladder Diagram

TIP:
The Sequence ID parameter can be a STRING tag in which the identifier is stored, or a quoted string containing up to 82 characters
Structured Text
if (SasiControl) then
SASI(Make_Product_101, IdString, Result);
end_if
Provide Feedback