Phase Command (PCMD)
This instruction applies to the Compact GuardLogix 5370 and Compact GuardLogix 5380, CompactLogix 5370, CompactLogix 5380, and CompactLogix 5480, ControlLogix 5570 and ControlLogix 5580, and GuardLogix 5570 and GuardLogix 5580 controllers.
TIP:
When using this instruction with ControlLogix redundancy system, outputs controlled by this instruction may not be bumpless during redundancy switchover, if the instruction and phase program are not scheduled in the highest priority task.
Use the PCMD instruction to change the state or sub-state of an equipment phase.
In the running state routine, use the PSC instructions to transition the equipment phase to the complete state. For more information about Paused functionality, please see the PPD phase instruction.
- This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
TIP:The PPD instruction is necessary for using pause functionality.

Number | Description |
|---|---|
![]() | Command Some states need a command to go to the next state. If the equipment phase is in the idle state, a start command transitions the equipment phase to the running state. Once in the running state, the equipment phase executes its running state routine. |
![]() | Other states use a Phase State Complete (PSC) instruction to go to the next state. If the equipment phase is in the holding state, a PSC instruction transitions the equipment phase to the held state. Once in the held state, the equipment phase needs a restart command to go to the restarting state. |
![]() | Sub-state Use Auto Pause, Pause, and Resume to test and debug a state routine. The sub-states require the Equipment Phase Paused (PPD) instruction to create breakpoints in the logic. Use the auto pause, pause, and resume commands to step through the breakpoints. |
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
PCMD (PhaseName,Command,Result);
Operands
Ladder Diagram
Operand | Type | Format | Description |
|---|---|---|---|
Phase Name | PHASE | Name of the equipment phase | Equipment phase to change to a different state. |
Command | command | Command enumeration value | Command to send to the equipment phase to change its state. For available commands, refer to the illustration above. |
Result | DINT | immediate tag | To let the instruction return a code for its success or failure, enter a DINT tag in which to store the result code. Otherwise, enter 0. |
Structured Text
The operands are the same as those for the Ladder Diagram PCMD instruction.
Guidelines for using the PCMD Instruction
Guideline | Details | |
|---|---|---|
Limit execution of a PCMD instruction to a single scan. | Limit the execution of the PCMD instruction to a single scan. Each command applies to only a specific state or states. Once the equipment phase changes state, the command is no longer valid. To limit execution, use methods such as:
| |
Determine if need ownership of the equipment phase. | As an option, a program can own an equipment phase. This prevents another program or FactoryTalk Batch software from also commanding the equipment phase. | |
If using: | Then: | |
FactoryTalk Batch software to also run procedures (recipes) within this controller | Also run procedures (recipes) within this controller. Before using a PCMD instruction, use an Attach to Equipment Phase (PATT) instruction to take ownership of the equipment phase. | |
Multiple programs to command the same equipment phase | Use an Attach to Equipment Phase (PATT) instruction to take ownership of the equipment phase. | |
None of the above | There is no need to own the equipment phase. | |
Using a POVR instruction instead of a PCMD instruction. |
For example, suppose the equipment checks for jammed material. And if there is a jam, the equipment should always abort. In that case, use the POVR instruction. This way, the equipment aborts even if under manual control via Logix Designer . | |
Determine if need a return code. | Use the Result operand to get a code that shows the success or failure of the PCMD instruction. | |
If: | Then in the Result operand, enter a: | |
Anticipate ownership conflicts or other possible errors | DINT tag, in which to store a code for the result of the execution of the instruction. | |
Do not anticipate ownership conflicts or other possible errors | 0 | |
Want to interpret the result code, refer to the Result Codes table below. | ||
PCMD Result Codes
If assigning a tag to store the result of a PCMD instruction, the instruction returns one of these codes when it executes:
Code (Dec) | Description |
|---|---|
0 | Successful command. |
24577 | Valid command. |
24578 | Invalid command for the current state of the equipment phase. For example, if the equipment phase is in the running state, then a start command is not valid. |
24579 | Cannot command the equipment phase. One of these already owns the equipment phase.
|
24594 | Unscheduled or inhibited equipment phase or in an inhibited task. |
TIP:
High priority HMI ownership is specific only to
CompactLogix
5370 and ControlLogix
5570 controllers.Affects Math Status Flags
No
Major/Minor Faults
None. See
Index Through Arrays
for operand-related faults.Execution
For Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic, it will execute. All conditions below the think solid line can only occur during Normal Scan mode.
Condition/State | Action Taken |
|---|---|
Prescan | No action taken. |
Postscan | No action taken. |
EnableIn is false | No action taken. |
EnableIn is true | The instruction executes as described above. |
Example 1
Ladder Diagram

Number | Description |
|---|---|
![]() | If ProcedureB_Stepindex = 20 (the routine is at step 20) And this is the transition to step 20 (the ONS instruction signals that the EQU instruction went from false to true.) Then Change the state of the Add_Water equipment phase to running via the start command. |
![]() | If ProcedureB_Stepindex = 20 (the routine is at step 20) And the Add_Water equipment phase is complete (Add_Water.Complete = 1) Then Change the state of the Add_Water equipment phase to resetting via the reset command. Advance to step 30. |
Structured Text

Number | Description |
|---|---|
![]() | When the SFC enters Add_Water_Step , change ADD_Water equipment phase to running via the start command, The P1 qualifier limits this to the first scan of the step. |
![]() | Before the SFC leaves Add_Water_Step (Add_Water_Complete = 1), change Add_Water equipment phase to resetting via the reset command. The P0 qualifier limits this to the last scan of the step. |
Example 2
Ladder Diagram

NOTE:
If ProcedureB_Stepindex = 30 (the routine is at step 30)
And this is the transition to step 30 (the ONS instruction signals that the EQU instruction went from false to true.)
Then
Change the state of the Add_Water equipment phase to running via the start command.
Verify that the command was successful and store the result code in PCMD_Result[1] [DINT Tag].
Structured Text

NOTE:
When the SFC enters
Add_Ingredient_Step
- ChangeAdd_Ingredientequipment phase to running via the start commend.
- Verify that the command was successful and store the result code inPCDM_Result[2](DINT tag).
The P1 qualifier limits this to the first scan of the step.
Provide Feedback