Standard Initialization Faults
This table defines a list of standard faults associated with the Initialization Faults attribute.
Standard Initialization Fault Descriptions
Bit | Fault | Description |
|---|---|---|
0 | Reserved | This bit cannot be used since the Fault Code is defined by the associated fault bit number and Fault Code of 0 means no fault condition is present. |
1 | Boot Block Checksum Fault | Checksum or CRC error for Boot Block of CIP Motion device detected as part of Self-Test. |
2 | Main Block Checksum Fault | Checksum or CRC error for Main Block of CIP Motion device detected as part of Self-Test. |
3 | Nonvolatile Memory Checksum Fault | Checksum or CRC error for NV Memory of CIP Motion device detected as part of Self-Test. |
4...31 | Reserved |
Provide Feedback