Motor Test Configuration Attributes
These are the attributes that are associated with result status applied to a Motion Control Axis.
Motor Test Travel Limit
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - C | Set/SSV# | REAL | 0 | 0 | ![]() | Motor Units |
The Motor Test Travel Limit attribute is used by the Dynamic Motor Test service to limit the range of the axis travel during the test. For linear motors, Motor Unit = Meters. For rotary motors, Motor Unit = Revs.
Motor Test Speed
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - D | Set/SSV# | REAL | 0 | 0 | ![]() | Motor Units/Seconds |
The Motor Test Speed attribute determines the maximum speed allowed by the Dynamic Motor Test service during the test. For linear motors, Motor Unit = Meters. For rotary motors, Motor Unit = Revs.
Motor Test Torque
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - D | Set/SSV# | REAL | 100 | 0 | ![]() | % Motor Rated |
The Motor Test Torque attribute determines the maximum applied torque allowed by the Dynamic Motor Test service during the test.
Motor Test Data Valid
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Required - D | Set/GSV | USINT | 0 | - | - | Enumeration: 0 = False 1 = True 2-255 = reserved |
The Motor Test Data Valid attribute is set True by
Studio 5000 Logix Designer
configuration software when a Motor Test is executed successfully and the user Accepts the results of the test. This attribute is set False by Studio 5000 Logix Designer
configuration software whenever the Motor Data Source attribute is changed or whenever the values for Motor Rated Power, or Motor Rated Voltage, or Motor Rated Current are changed.The Motor Test Data Valid attribute is used by
Studio 5000 Logix Designer
configuration software to determine if factory defaults need to be calculated for motor model attributes.Provide Feedback