Frequency Control Signal Attribute
This attribute is the signal attribute associated with the Frequency Control method of operation of a Motion Control Axis.
Slip Compensation
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Required - F | Get | T | REAL | - | - | - | RPM |
Indicates the actual amount of slip compensation currently being applied.
Provide Feedback