Exception User Limit Config Attrib
These are the exception user limit configuration related attributes associated with a Motion Control Axis.
Motor Phase Loss Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XD | Set | REAL | 5 | 0 | 100 | % Motor Rated |
Sets the minimum motor phase current for the Motor Phase Loss exception. The current in each motor phase must exceed this value during the motor phase loss test or a Motor Phase Loss exception occurs. Decreasing this attribute's value lowers sensitivity to phase loss conditions. A value of 0 will effectively disable the motor phase loss test.
Motor Overspeed User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - D | Set | REAL | FD | 0 | ![]() | % Motor Rated |
Sets the Overspeed User Limit relative to the Rotary Motor Rated Speed or Linear Motor Rated Speed that is allowable before throwing a Motor Overspeed UL exception.
Motor Overtemperature User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XD | Set | REAL | FD | 0 | ![]() | o C |
Sets User Limit for the Motor Overtemperature UL exception.
Motor Thermal Overload User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XD | Set | REAL | 110 | 0 | ![]() | % Motor Rated |
Sets User Limit for the Motor Thermal Overload UL exception.
Inverter Overtemperature User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XD | Set | REAL | o C |
Sets User Limit for the Inverter Overtemperature UL exception.
Inverter Thermal Overload User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XD | Set | REAL | 110 | 0 | ![]() | % Inverter Rated |
Sets User Limit for the Inverter Thermal Overload UL exception.
Inverter Ground Current User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XD | Set/SSV | REAL | 110 | 0 | ![]() | % Factory Limit |
Sets the User Limit for the Inverter Ground Current UL exception as a percentage of the Inverter Ground Current Factory Limit.
Converter Overtemperature User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - BD | Set | REAL | 0 | 0 | ![]() | C |
Sets User Limit for the Converter Overtemperature UL exception.
Converter Thermal Overload User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - BD | Set | REAL | 100 | 0 | ![]() | % Converter Rated |
Sets User Limit for the Converter Thermal Overload UL exception.
Converter Ground Current User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set/SSV | REAL | 100 | 0 | ![]() | % Factory Limit |
Sets User Limit for the Converter Ground Current UL exceptionas a percentage of the Converter Ground Current Factory Limit.. .
Bus Regulator Overtemperature User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XBD | Set | REAL | C |
Sets User Limit for the Bus Regulator Overtemperature UL exception.
Bus Regulator Thermal Overload User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XBD | Set | REAL | % Regulator Rated |
Sets User Limit for the Bus Regulator Thermal UL exception.
Bus Overvoltage User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XBD | Set | REAL | % Nominal Bus Voltage |
Sets User Limit for the Bus Overvoltage UL exception. Unlike the corresponding Factory Limit, which is specified in Volts, the User Limit is based on percent of Nominal Bus Voltage during operation.
Bus Undervoltage User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XBD | Set | REAL | % Nominal Bus Voltage |
Sets User Limit for the Bus Undervoltage UL exception. Unlike the corresponding Factory Limit, which is specified in Volts, the User Limit is based on percent of Nominal Bus Voltage during operation.
Converter Pre-Charge Overload User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set/SSV | REAL | 100 | 0 | ![]() | % Converter Rated |
Sets User Limit for the Converter Pre-Charge Overload UL exception.
Feedback Noise User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - E | Set | UDINT | 1 | 1 | 2 31 | Noise Counts |
Sets User Limit for the Feedback Noise Overload UL exception. Example of Noise Counts would be simultaneous transitions of the A and B channel of a quadrature encoder feedback device.
Feedback Signal Loss User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - E | Set | REAL | 100 | 0 | ![]() | % FL Voltage Drop |
Sets User Limit for the Feedback Signal Loss UL exception. Feedback interface hardware typically monitor average voltage levels on incoming signals. Feedback Signal Loss conditions occur when the average voltage levels drop below a percentage of voltage drop allowed by the Feedback Signal Loss Factory Limit.
Feedback Data Loss User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - E | Set | UDINT | 4 | 1 | 2 31 | Consecutive Lost Data Packets |
Sets User Limit for the Feedback Data Loss UL exception. For digital feedback devices, feedback interface hardware monitors the integrity of data transferred over the serial connection to the feedback device. Feedback Data Loss conditions occur when two or more consecutive data packets are lost or corrupted.
Control Module Overtemperature User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - All | Set | REAL | C |
Sets User Limit for the Control Module Overtemperature UL exception.
Converter Pre-Charge Overload User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - XBD | Set | REAL | % Rated |
Sets User Limit for the Converter Pre-Charge Overload UL exception.
AC Line Overvoltage User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 110 | 0 | ![]() | % Rated |
Sets the high voltage limit as a percent of Converter Rated Input Voltage for the AC line source.
AC Line Undervoltage User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0 | 0 | 100 | % Rated |
Sets the low voltage limit as a percent of Converter Rated Input Voltage for the AC line source.
AC Line Overvoltage User Limit - Alternate
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 110 | 0 | ![]() | % Rated |
Sets the high voltage limit as a percent of Converter Rated Input Voltage for the alternate AC line source.
AC Line Undervoltage User Limit - Alternate
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0 | 0 | 100 | % Rated |
Sets the low voltage limit as a percent of Converter Rated Input Voltage for the alternate AC line source.
AC Line High Freq User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0.4 | 0 | ![]() | Hertz |
Sets the high frequency limit as the difference from the nominal AC line frequency.
AC Line Low Freq User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0.7 | - ![]() | 0 | Hertz |
Sets the low frequency limit as the difference from the nominal AC line frequency.
AC Line High Freq User Limit - Alternate
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0.4 | 0 | ![]() | Hertz |
Sets the high frequency limit as the difference from the nominal alternate AC line source frequency.
AC Line Low Freq User Limit - Alternate
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0.7 | - ![]() | 0 | Hertz |
Sets the low frequency limit as the difference from the nominal alternate AC line source frequency.
Converter Heatsink Overtemperature User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 125 | 0 | ![]() | C |
Sets a User Limit for the regenerative converter power structure heatsink temperature. Exceeding this value generates a Converter Overtemperature UL exception.
AC Line Overload User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 110 | 0 | ![]() | % Converter Rated |
Sets a User Limit for thermal overload of Line 1, 2, and 3 components as a percent of their rated thermal capacity. Exceeding this value generates a Converter Thermal Overload UL exception.
AC Line Resonance User Limit
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 12 | 0 | 100 | % Converter Rated |
Sets the User Limit for the AC Line Resonance UL exception based on a percentage of the Converter Output Rated Current. The AC Line Resonance UL exception occurs when the current flowing through the AC line filter in the resonant frequency band, exceeds the user limit for a vendor specified period.
Provide Feedback

C