Converter Output Attributes
These are the converter output related attributes associated with Motion Control Axis.
Converter Output Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | T | REAL | - | - | - | Amps |
The Converter Output Current attribute is the output current generated by the Bus Converter. A positive value indicates current flow out of the converter, where the converter is supplying DC bus power to attached loads. A negative value indicates current flow into the converter, where the converter is absorbing “regenerative” power from attached loads.
Converter Output Power
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | T | REAL | - | - | - | Kilowatts |
The Converter Output Power attribute is the output power generated by the Bus Converter. This value is based on the product of the Converter Output Current and DC Bus Voltage. A positive value indicates power flow out of the converter, where the converter is supplying DC bus power to attached loads. A negative value indicates power flow into the converter, where the converter is absorbing "regenerative" power from attached loads.
Provide Feedback