Converter Current Ref Config Attrib
These are the current reference configuration attributes associated with a Regenerative Converter.
System Capacitance
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Required - G Voltage Control only | Set/SSV | REAL | 0 FD | 0 | ![]() | % Rated (Volts/Second) |
The System Capacitance attribute is the scaling gain value that converts voltage rate commanded by the bus voltage control loop into equivalent active current, expressed as a percent of the converter's current rating. Properly set, this value represents the total system capacitance of the DC bus.
Active Current Command
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0 | - ![]() | ![]() | % Rated |
The Active Current Command attribute sets the reference current used to actively regulate the Active Current of the converter when in the Running state and configured for AC Line Current Control mode. A positive value implies motoring current. A negative value implies regenerative current.
Reactive Current Command
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0 | - ![]() | ![]() | % Rated |
The Reactive Current Command attribute sets the reference current used to actively regulate the Reactive Current of the converter when in the Running state and configured for AC Line Current Control mode. A positive value implies reactive current (lagging relative to voltage) is consumed by the converter. A negative value implies reactive current (leading relative to voltage) is produced by the converter.
Active Current Trim
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set/ | REAL | 0 | - ![]() | ![]() | % Rated |
The Active Current Trim attribute is the additional current command added to the active current reference summing junction.
Active Current Low Pass Filter Bandwidth
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0 FD | 0 | 10 4 | Radians/Sec |
The Active Current Low Pass Filter Bandwidth attribute is the break frequency for the low pass filter applied to active current reference signal. A value of 0 for this attribute disables this feature.
Active Current Notch Filter Frequency
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 0 | 0 | 10 4 | Radians/Sec |
The Active Current Notch Filter Frequency attribute is the center frequency of the notch filter applied to the active current reference signal. A value of 0 for this attribute disables this feature.
Active Current Rate Limit
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 100 | 0 | ![]() | % Rated/Second |
The Active Current Rate Limit attribute sets the magnitude limit on the rate of change of the converter's active current reference signal. This attribute applies only when configured for AC Line Current Control mode.
Reactive Current Rate Limit
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set | REAL | 100 | 0 | ![]() | % Rated/Second |
The Reactive Current Rate Limit sets the magnitude limit on the rate of change of the converter's reactive current reference signal. This attribute applies only when configured for AC Line Current Control mode.
Kc
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Required - G Voltage Control only | Set | REAL | - | - | - | % Rated/(Volts/Second) |
The Kc attribute is the scaling gain value that converts voltage rate commanded by the bus voltage control loop into equivalent active current, expressed as a percent of the converter’s current rating. Properly set, this value represents the total system capacitance of the DC bus.
Provide Feedback