Convert AC Line Source Config Attrib
These are the converter AC Line source configuration attributes associated with the AC Line input to a Converter.
AC Line Source Select
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set/SSV | USINT | 0 | - | - | Enumeration: 0 = AC Line A 1 = AC Line B (Alternate) 2-255 = Reserved |
The AC Line Source Select attribute determines which AC Line source is active for the converter and applies the configured impedance and power rating of that source to the converter's control structure.
AC Line Source Impedance
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set/SSV | REAL | 5 | 0 | 100 | % Rated Impedance |
The AC Line Source Impedance attribute determines the impedance of the AC line source as a percent of the transformer or generator impedance rating.
AC Line Source Power
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set/SSV | REAL | 2500 10*Converter Rated Power | 0 | ![]() | kVA |
The AC Line Source Power attribute sets the power rating of the transformer or generator feeding power to the converter as a percentage of the converter's power rating.
AC Line Source Impedance - Alternate
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set/SSV | REAL | 5 | 0 | 100 | % Rated Impedance |
The AC Line Source Impedance - Alternate attribute determines the impedance of the alternate AC line source as a percent of the transformer or generator impedance rating.
AC Line Source Power - Alternate
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - G | Set/SSV | REAL | 100 10*Converter Rated Power | 0 | ![]() | kVA |
The AC Line Source Power - Alternate attribute selects the power rating of the alternate transformer or generator feeding power to the converter as a percentage of the converter's power rating.
Provide Feedback