Axis Statistical Attributes
These are the attributes that provide useful statistics on motion axis operation.
Control Power-up Time
Usage | Access | T | Data Type | Default | Min | Max | Semantics of value |
|---|---|---|---|---|---|---|---|
Optional - XBD | Get/GSV | REAL | - | - | - | Seconds |
Elapsed time since the axis control power was last applied.
Cumulative Run Time
Usage | Access | T | Data Type | Default | Min | Max | Semantics of value |
|---|---|---|---|---|---|---|---|
Optional - XBD | Get/GSV | REAL | - | - | - | Hours |
Accumulated time that the axis has been powering the Running state.
Cumulative Energy Usage
Usage | Access | T | Data Type | Default | Min | Max | Semantics of value |
|---|---|---|---|---|---|---|---|
Optional - XBD | Get/GSV | REAL | - | - | - | Kilowatt Hours |
Accumulated output energy of the axis.
Cumulative Motor Rev
Usage | Access | T | Data Type | Default | Min | Max | Semantics of value |
|---|---|---|---|---|---|---|---|
Optional - D | Get/GSV | LINT | - | - | - |
Cumulative number of times the motor shaft has turned. (Rotary Motors Only).
Cumulative Main Power Cycles
Usage | Access | T | Data Type | Default | Min | Max | Semantics of value |
|---|---|---|---|---|---|---|---|
Optional - XBD | Get/GSV | DINT | - | - | - |
Cumulative number of times AC Mains has been cycled.
Cumulative Control Power Cycles
Usage | Access | T | Data Type | Default | Min | Max | Semantics of value |
|---|---|---|---|---|---|---|---|
Optional - XBD | Get/GSV | DINT | - | - | - |
Cumulative number of times Control Power has been cycled.
Cumulative Control Power-Up Time
Usage | Access | T | Data Type | Default | Min | Max | Semantics of value |
|---|---|---|---|---|---|---|---|
Optional - XBD | Get/GSV | REAL | - | - | - | Hours |
Accumulated time that control power has been applied.
Provide Feedback