Axis Info Attributes
These are the attributes that provide information about the associated hardware capabilities of the Motion Control Axis.
Inverter Rated Output Voltage
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Required - D Optional - X !LTM | Get | REAL | - | - | - | Volts (RMS) |
The Inverter Rated Output Voltage attribute is the drive inverter output voltage rating. This value is hard coded in the device.
Inverter Rated Output Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Required - D Optional - X !LTM | Get | REAL | - | - | - | Amps (RMS) |
The Inverter Rated Output Current attribute is the drive inverter output current rating. This value is hard coded in the device.
Inverter Rated Output Power
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Required - D Optional - X !LTM | Get | REAL | - | - | - | Kilowatts |
The Inverter Rated Output Power attribute is the drive inverter output power rating. This value is hard coded in the device.
Converter Rated Output Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | REAL | - | - | - | Amps |
The Converter Rated Output Current attribute is the converter output current rating.
Converter Rated Output Power
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | REAL | - | - | - | Kilowatts |
The Converter Rated Output Power attribute is the converter output power rating.
Converter Rated Output Voltage
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | REAL | - | - | - | Volts |
The Converter Rated Output Voltage attribute is the converter output voltage rating.
Converter Rated Input Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | REAL | - | - | - | Amps (RMS) |
The Converter Rated Input Current attribute is the converter input current rating.
Converter Rated Input Power
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | REAL | - | - | - | Kilowatts |
The Converter Rated Input Power attribute is the converter input power rating.
Converter Rated Input Voltage
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | REAL | - | - | - | Volts (RMS) |
The Converter Rated Input Voltage attribute is the converter input voltage rating.
Drive Power Structure Axis ID
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - D | Get | UDINT | - | - | - | ID# |
The Drive Power Structure Axis ID attribute identifies the power structure with the axis instance.
Provide Feedback