Rockwell Automation Specific CIP Axis Alarm Names
The following table lists the resulting Alarm names associated with the Rockwell Automation specific exception conditions.
Bit | Object CIP Axis Alarm Name |
|---|---|
1 | Commutation Startup Alarm |
4 | Feedback Filter Noise Alarm |
5 | Feedback Battery Loss Alarm |
6 | Feedback Battery Low Alarm |
7 | Feedback Incremental Count Error Alarm |
10 | Control Module Overtemperature FL Alarm |
11 | Control Module Overtemperature UL Alarm |
12 | Converter Pre Charge Overload FL Alarm |
13 | Converter Pre-Charge Overload UL Alarm |
14 | Excessive Current Feedback Offset Alarm |
15 | Regenerative Power Supply Alarm |
16 | PWM Frequency Reduced Alarm |
17 | Current Limit Reduced Alarm |
18 | Torque Prove Alarm |
19 | Decel Override Alarm |
20 | Preventative Maintenance Alarm |
21 | Motor Test Alarm |
22 | Hardware Configuration Alarm |
23 | Firmware Change Alarm |
24 | Converter Pre-Charge Input Deactivated Alarm |
25 | DC Common Bus Alarm |
26 | Runtime Error Alarm |
27 | Backplane Communication Error Alarm |
28 | Safety Module Communication Error Alarm |
29 | AC Line Contactor Alarm |
30 | AC Line Resonance FL Alarm |
31 | AC Line Resonance UL Alarm |
53 | Excessive Motor Voltage Feedback Offset Alarm |
63 | Product Specific Alarm |
Provide Feedback