Solutions
Solutions in your vault can be used to organize automation system projects. Solutions group together a collection of controller project files that interact together as a system. For example, solutions can be defined by the different machines in your factory, process areas in your plant, or however a system is defined.
NOTE:
FactoryTalk Vault uses stateful urls. This allows you to bookmark or share specific content with other users in an organization by selecting the url displayed in the address bar.
Your vault contains a default solution that you can use to get started.
Add a solution to your vault
- From the vault, click the drop-down arrow next toADD.
- SelectCreate Solution.
- In theCreate Solutiondialog box complete these items:
- Name- Required. The name:
- Must be between 1 and 200 characters
- Cannot start or end with whitespace, that is, cannot start or end with a space or tab.
- Cannot contain any invisible control characters such as new line, bell, tab, etc...
- Cannot contain folder separator characters such as slah or backslash.
- Should be unique within the current scope of the project, whether solution or folder.
- Description- Optional.
The solution appears in the navigation pane of your vault.
Add projects to a solution
- From the vault navigation pane, select the solution to which you want to add projects.
- In the center pane, selectAdd projects (s) to <SolutionName>.
- ClickSELECT FILESto display theFile Uploaddialog box.
- Select the project files to add.
- SelectOpento add the projects to the solution. TheAdd Projectspanel displays to show the project properties.TIP: If there are any naming conflicts in the projects, rename the projects or remove the projects from the solution in theAdd Projectspanel.
- SelectSaveto start uploading the selected projects.
The solution list displays the projects and their status.
Upgrade solution projects
- From the vault navigation pane, select the solution in which you want to upgrade projects.TIP: Select the checkbox in the header row to upgrade all projects in the solution.
- In the vault toolbar, selectUpgrade.
- In theUpgrade Logix Projectwindow, underSelect Logix Versionselect the Logix version to which you want to upgrade the solution’s projects.NoteThe projects in the solution that can be upgraded will be selected. You can clear the selection from any projects in the solution that you don’t want upgraded. Projects that cannot be upgraded appear dimmed in the list.
- SelectContinue
- InReview Warningsreview the list of potential impacts of upgrading the projects. To continue the upgrade, clickUpgrade.
The project list displays the progress of the upgrade.
Download solution projects
- From the vault navigation pane, select the solution from which you want to download projects.
- Select the checkboxes of the projects to download.TIP: Select the checkbox in the header row to download all projects in the solution.
- In the vault toolbar, selectDownload.
- From the list, select which type of project file to download, then slectDownload.
- The download starts.
- If prompted, clickYesto allow the download.
- The projects in the solution are downloaded to your defaultDownloadfolder.
Move a project
You can move projects between your personal tenant and your organization as well as move them between solutions.
- From the vault navigation pane, select the solution from which you want move the project.
- Select the checkbox for the project you want to move.
- In the vault toolbar, selectMoveto open theMove Projectdialog box.
- UnderSelect Organizationclick the down arrow and select the destination organization.
- UnderSelect Solutionclick the down arrow and select the destination solution.
- ClickMove.
Delete a solution
Deleting a solution removes all controller projects within the solution.
- From the vault navigation pane, select the solution to delete.
- In the vault toolbar, selectDelete.
- In theDelete solutionconfirmation dialog, clickDelete.
The solution is removed from the vault. Click
to view the item in the
Trash
Trash
.Edit solution properties
- From the vault navigation pane, select the solution.
- In the vault toolbar, selectSolution Properties.
- Click theEditpencil
next to the name of the solution to change the solution name. - Click theEditpencil
next the description of the solution to change the solution description. - ClickSaveto apply the changes.TIP: TheSAVEbutton is enabled if there are unsaved changes. If you close the panel without saving the changes are discarded.
Provide Feedback