Roles in FactoryTalk Vault
This section shows the capabilities of the different roles a user can be assigned when working with FactoryTalk Vault.
NOTE:
FactoryTalk Vault has 2GB of storage included by default. An entitlement can be purchased which provides 250GB of storage.
The roles a user can be assigned are:
- Viewer - User can access data in FactoryTalk Vault but cannot upload, modify, or download anything from FactoryTalk Vault.
- Consumer - User can download files in addition to ability to access data that Viewer has.
- Contributor - User can upload, modify, and delete files.
- Admin - User has full abilities to access, upload, modify, and delete files as well as add and remove other users.
Role | Admin | Modify | View | Analyze | Download |
|---|---|---|---|---|---|
Viewer | X | X | |||
Consumer | X | X | X | ||
Contributor | X | X | X | X | |
Admin | X | X | X | X | X |
Provide Feedback