Tiers
Twin Studio allows the user to select the tier to use based on their project requirements, the different tiers provide different performance and machine requirements. Credits are spent accordingly. Twin Studio supports the following tiers by application:
Studio 5000 Logix Designer : large tier only
Large | |
|---|---|
Cost | 3 credits per hour |
CPUs | 8 |
Memory | 32 GB |
Emulate 3D: small, medium and large tier
Small | Medium | Large | |
|---|---|---|---|
Cost | 6 credits per hour | 8 credits per hour | 10 credits per hour |
CPUs | 8 | 32 | 64 |
Memory | 32 GB | 128 GB | 256 GB |
Arena: small, medium and large tier
Small | Medium | Large | |
|---|---|---|---|
Cost | 4 credits per hour | 5 credits per hour | 6 credits per hour |
CPUs | 2 | 4 | 8 |
Memory | 8 GB | 16 GB | 32 GB |
Provide Feedback